We are using P2040 in our board. We are using QorIQ SDK V2.0 along with update 
SDK-v2.0-1703 .
In QorIQ SDK v2.0-1703 Documentation in Table 59. NOR Flash Memory Map is Given .
How to customise this memory map if we want to use root file system with more than 44MB size
Is there any place in the code or compile environment where I have to make the changes for enlarging the rootfs from 0xe9300000 - 0xebefffff to 0xe8900000 - 0xebefffff .
We have directly connected the msb ( A25 pin ) pin of flash to processor address, LA5 . Which means we will not have alternate bank concept in our design.
In this case can we enlarge our rootfs from 0xe8900000 to 0xefefffff ..?
Hello k aravind vijaya kumar,
If you don't use Hypervisor, you could enlarge rootfs filesystem from 0xe8900000 to 0xebefffff.
Thanks,
Yiping