How many devices can be handled by PCI express controller of p2041

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many devices can be handled by PCI express controller of p2041

3,327 Views
sameerarvikar
Contributor III

P2041 is having 3 PCI express controller

I am using PEX2 (PCI Express Controller 2)

Is there any limit of number of PCI devices that can be connected to PCI Express controller

or we can connect any number of devices using switches and bridges

Thanks and regards

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,607 Views
ufedor
NXP Employee
NXP Employee

According to the PCI Express Specification a device's location for a PCIe controller is specified by an 8-bit bus number, a 5-bit device number and a 3-bit function number.

0 Kudos
Reply

2,607 Views
sameerarvikar
Contributor III

As per P2041 reference manual (Table 24.1 and Table 24.3)

PEX2(PCI express controller )

INTA has got Interrupt number 25

INTB has IRQ5,

INTC has IRQ6

INTD has IRQ7

So does that mean it can support only 4 pci devices ?

0 Kudos
Reply

2,607 Views
ufedor
NXP Employee
NXP Employee

PCIe devices use MSI interrupts.