GDB Server support on QorIQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GDB Server support on QorIQ

2,393 Views
ugendreshwarkud
Contributor II

To enable GDB server on any QorIQ platform you need the following components:

  1. gdbserver tool running on QorIQ platform
  2. gdb tool running on host system that support QorIQ targets and connects to gdbserver

The gdbserver tools comes as part of the gdb package itself and the command to build it in Yocto SDK is "bitbake gdb".

And the command to build gdb for host system usage is "bitbake gdb-cross" and the binary is installed at "<Yocto SDK Home>/build_<platfrom_rdb>_release/tmp/sysroots/i686-linux/usr/bin/ppce5500-fsl-linux/powerpc-fsl-linux-gdb.

You can refer to the below link on the usage of GDB server

Cross debugging with GDB | STLinux


For GDB tool documentation please refer to the below link:


Debugging with GDB: Top

Tags (3)
0 Kudos
Reply
0 Replies