Corenet fabric speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Corenet fabric speed

1,981 Views
Simbu
Contributor II

Hi All,

In past, I think the FSB (Front Side Bus/Bus Speed) for any processor is computed against half the clock rate, so for e.g. 1.8 GHz processor with dual 32 Bit bus , both clocked at 450 Mhz. If I use the same concept here(p4080 -1.5 Ghz) in case of fabric and assume the fabric is accelerated @ ~750 Mhz .

Is this assumption right? It would be great, if someone can clarify how can we correlate the bus speed against fabric speed?

Any specific document or reference link will also be helpful..

Thanks in Advance.

Labels (1)
0 Kudos
Reply
2 Replies

1,669 Views
Simbu
Contributor II

I found the below statement from P4080 product description link

Power management is always a major design consideration in embedded applications, and for this reason,

the P4080 is designed to dissipate <30 W Max with all 8 CPUs and platform logic running at maximum

frequency (8x 1.5 GHz CPUs, 800 MHz CoreNet).

Does this mean that the corenet speed as such one and can't be described against single core like speed/core ??

Thanks in Advance.

0 Kudos
Reply

1,669 Views
Simbu
Contributor II

Thanks.. I got the answer from U boot log and from the uboot code freqSystemBus.

0 Kudos
Reply