Assign memory address to DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assign memory address to DDR

Jump to solution
1,849 Views
敏赵
Contributor I

Hi,

The size of my DDR chip is 4GB, can I only assign 1GB memory address to it?

Best regards,

Min Zhao

Labels (1)
0 Kudos
Reply
1 Solution
1,674 Views
catalindemergia
Contributor IV

Yes, you have to specify:

the base address that you want from Local Access Window Base Address Register

the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31

regards,

Catalin

View solution in original post

0 Kudos
Reply
1 Reply
1,675 Views
catalindemergia
Contributor IV

Yes, you have to specify:

the base address that you want from Local Access Window Base Address Register

the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31

regards,

Catalin

0 Kudos
Reply