P2040/P2041 Pre-Boot Loader/Boot Sequencer Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2040/P2041 Pre-Boot Loader/Boot Sequencer Specific FAQs

P2040/P2041 Pre-Boot Loader/Boot Sequencer Specific FAQs

I wanted to choose boot location for P2040. Does P2040 supports GPCM 16 bit NOR boot?

Yes, P2040 supports GPCM 16 bit NOR boot. It can be done by configuring 4 bits (bit 192 to 195) of RCW source location to 1101.


If I use NOR FLASH as boot device, can NOR FLASH be used as RCW storage device? Do I need an extra SPI flash is required or not?

Yes, you can use NOR flash and the options are 0x1100 and 0x1101 (listed in the table 4-26 in P2040 Reference Manual).


Does P2040 support to boot from SPI flash?

Yes, P2040 can boot from SPI flash. But it is different from booting from NOR flash. One eSPI pre-bootloader is required.



ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎08-06-2012 10:15 AM
更新者: