P2010/P2020 eSDHC Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2010/P2020 eSDHC Specific FAQs

P2010/P2020 eSDHC Specific FAQs

Can you please share throughput numbers for P2010 and eSDHC interface?

The basic data rate is 200MB/s for SD/MMC cards using 4 parallel lanes and 416Mbps for MMC using 8 parallel lanes


For P2010/P2020, is the SD device / card handled as a block device as it is for Compact flash device? If handled as block device is that implemented by internal logic or should it be implemented in sw / fw?

Yes, P2010/P2020 is handled as a block device and it does single or multi-block read/writes. This is handled by internal logic and is set up via the eSDHC register set through the drivers.


Does P2010/P2020 eSDHC interface support a SDHC card above 4GB?

Yes, eSDHC interface does support a SDHC card above 4GB. The eMMC standard is introduced in JESD84-A44. The new features of the eMMC that eSDHC does not support, are not supported. However, the basic operation of the MMC card is supported.



ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎08-06-2012 09:50 AM
更新者: