P1024/P1015 Ethernet Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1024/P1015 Ethernet Specific FAQs

P1024/P1015 Ethernet Specific FAQs

How can I ensure that Ethernet flow control is turned on through the register setting in P1015?

Please try the below steps to enable Ethernet flow control: 1) Set MACCFG1[Rx_Flow] && MACCFG1[Tx_Flow] to 1 2) Set RCTRL[LFC] to 1. Setting the flow control bits Rx_Flow and Tx_Flow means that the MAC can detect and act on PAUSE flow control frames, receive and transmit respectively. There are two ways you can confirm or see them in action: 1) Software sending a PAUSE frame through TCTRL[TFC_PAUSE] 2) Changing some hidden FIFO threshold registers, such that the FIFO is about to overflow and that triggers eTSEC logic to send a PAUSE.


ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎08-06-2012 09:29 AM
更新者: