xen hypervisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

xen hypervisor

2,912 Views
nayannick
Contributor I

I am trying to build xen hypervisor for imx8m plus board through  yocto [zeus branch],
I was following the AN13138 document by nxp [Xen Deployment on Layerscape Platforms],

However i am stuck at 2.2.1 Run Xen and Dom0 where board is not booting with xen image ,through yocto i got xen and xen.efi only two images with xen name, is it wright images

1)Is there any document for xen deployment for imx8mp particularly ?, if not which one i can use which is close to it,
2)what are the modification required at U-boot and kernel level for xen ?, can you suggest anything related to it 

Tags (2)
0 Kudos
Reply
2 Replies

2,881 Views
nayannick
Contributor I
BSP-Yocto-NXP-i.MX8MP-PD23.1.0
Linux NXP Vendor Kernel v5.15.71_2.2.2-phy3 (based on NXP tag lf-5.15.71-2.2.2)

  Yocto 4.0.13 (Kirkstone)   

 is it work for this version ?

0 Kudos
Reply

2,897 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Which BSP version are you using? XEN is not supported in MX8MPlus since 4.14.88 kernel.

Regards

0 Kudos
Reply