xen hypervisor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

xen hypervisor

2,890件の閲覧回数
nayannick
Contributor I

I am trying to build xen hypervisor for imx8m plus board through  yocto [zeus branch],
I was following the AN13138 document by nxp [Xen Deployment on Layerscape Platforms],

However i am stuck at 2.2.1 Run Xen and Dom0 where board is not booting with xen image ,through yocto i got xen and xen.efi only two images with xen name, is it wright images

1)Is there any document for xen deployment for imx8mp particularly ?, if not which one i can use which is close to it,
2)what are the modification required at U-boot and kernel level for xen ?, can you suggest anything related to it 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,859件の閲覧回数
nayannick
Contributor I
BSP-Yocto-NXP-i.MX8MP-PD23.1.0
Linux NXP Vendor Kernel v5.15.71_2.2.2-phy3 (based on NXP tag lf-5.15.71-2.2.2)

  Yocto 4.0.13 (Kirkstone)   

 is it work for this version ?

0 件の賞賛
返信

2,875件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Which BSP version are you using? XEN is not supported in MX8MPlus since 4.14.88 kernel.

Regards

0 件の賞賛
返信