-

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
2,404 次查看
ymha07
Contributor II

Moved to P series forum

==========================================================================

Wireless 1588 communications with P2020RDB-PCA

Hi, 

I want to try to construct a Wireless LAN using P2020RDB-PCAs with QorIQ SDK 1.9.

However, it seems difficult to find available wireless modules and drivers that support the platform.

Could you please recommend modules and drivers?

Moreover, is it possible to use IEEE 1588 hardware time stamping for wireless communications? 

Or do I have to use software time stamping?

Thanks in advance for your help.

 

 

标记 (2)
0 项奖励
回复
1 解答
2,374 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

在原帖中查看解决方案

2 回复数
2,375 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following link.

https://community.nxp.com/t5/QorIQ/after-install-ath10k-pci-module-on-ls1021a-TWR-Eva-wlp1s0-scan/m-...

 

In addition, it is impossible to use IEEE 1588 hardware time stamping for wireless communications

 

2,344 次查看
ymha07
Contributor II

Thank you for the reply.

I will refer to the link

0 项奖励
回复