ultra-wide AC or DC input to DC output SMPS circuit design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ultra-wide AC or DC input to DC output SMPS circuit design

612 次查看
Zaim
Contributor I

Hi,

 

I want to design an SMPS circuit with the following specifications:

 

 

* Input can be either 33-265 VAC or 48-375 VDC (ultra-wide input)

 

 

* Multiple DC outputs

 

1.output : 24V with 0.7 A

 

2.output : +10V with 0.8 A

 

1.output : -10V with 0.8 A

 

1.output : 5V with 0.5 A

 

1.output : 3.3V with 1 A

 

* Output power (40-100W)

 

 

.

 

 

How to design an isolated  power supply circuit with the specifications above ?

 

How can I make the transformer calculations according to this circuit? Is there any softwares to do that ? Please guide us 

 

sincerely,

 

Zaim.

 

 

0 项奖励
回复
1 回复

596 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Has replied to you based on your case.

0 项奖励
回复