ultra-wide AC or DC input to DC output SMPS circuit design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ultra-wide AC or DC input to DC output SMPS circuit design

611 Views
Zaim
Contributor I

Hi,

 

I want to design an SMPS circuit with the following specifications:

 

 

* Input can be either 33-265 VAC or 48-375 VDC (ultra-wide input)

 

 

* Multiple DC outputs

 

1.output : 24V with 0.7 A

 

2.output : +10V with 0.8 A

 

1.output : -10V with 0.8 A

 

1.output : 5V with 0.5 A

 

1.output : 3.3V with 1 A

 

* Output power (40-100W)

 

 

.

 

 

How to design an isolated  power supply circuit with the specifications above ?

 

How can I make the transformer calculations according to this circuit? Is there any softwares to do that ? Please guide us 

 

sincerely,

 

Zaim.

 

 

0 Kudos
Reply
1 Reply

595 Views
guoweisun
NXP TechSupport
NXP TechSupport

Has replied to you based on your case.

0 Kudos
Reply