tja1043 wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tja1043 wake up

1,279 Views
zhouqichen
Contributor I
 

hello,TJA1043T assumes that VBAT 24V, how much voltage is needed for the wake pin to wake up the CAN, and what connection method is available to make the wake wake up when connected to 9V

0 Kudos
Reply
1 Reply

1,269 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

A local wake-up event is triggered by a LOW-to-HIGH or HIGH-to-LOW transition on the WAKE pin since it has a bi-directional input threshold (falling or rising edge). The threshold voltage is specified in the datasheet, Table 8:

Capture.JPG

For more information, please take a closer look at the AH1014, Chapter 6.4 (Wake via pin WAKE).

Best regards,

Tomas

0 Kudos
Reply