the Bootloader for S32R45 run failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the Bootloader for S32R45 run failed

1,169 Views
aiweixin
Contributor IV

Hi,

    I install Platform_Software_Integration_S32R45_2022_03.exe, and import "Bootloader_S32R45_ASR_4.4_M7" project to EB.

    Then, i add "Spi" module to the project, and generate project.

    When configure "Config Variant" is "VariantPostBuild", the Bootloader.bin can load and run M7 app.

    But, configure "Config Variant" is "VariantPreCompile", the Bootloader.bin can't load and run M7 app, it occur "hard fault", enter "HardFault_Handler", then enter "MemManage_Handler".

aiweixin_0-1700811963519.png

     Why does it occur "hard fault"? And, how to solve it?

Best regards!

Tags (3)
0 Kudos
Reply
1 Reply

1,152 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Escalating this query to regional FAE.

Best regards,

Peter

0 Kudos
Reply