the Bootloader for S32R45 run failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the Bootloader for S32R45 run failed

1,158件の閲覧回数
aiweixin
Contributor IV

Hi,

    I install Platform_Software_Integration_S32R45_2022_03.exe, and import "Bootloader_S32R45_ASR_4.4_M7" project to EB.

    Then, i add "Spi" module to the project, and generate project.

    When configure "Config Variant" is "VariantPostBuild", the Bootloader.bin can load and run M7 app.

    But, configure "Config Variant" is "VariantPreCompile", the Bootloader.bin can't load and run M7 app, it occur "hard fault", enter "HardFault_Handler", then enter "MemManage_Handler".

aiweixin_0-1700811963519.png

     Why does it occur "hard fault"? And, how to solve it?

Best regards!

タグ(3)
0 件の賞賛
返信
1 返信

1,141件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Escalating this query to regional FAE.

Best regards,

Peter

0 件の賞賛
返信