smd code for freescale part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

smd code for freescale part

1,815 Views
lroth
Contributor I

I have a Freescale SMD part with the markings M933 VBGA. Would anyone know what this is? I can see from the circuit it is used in that it must be some sort of driver as it is driving two solenoids.

0 Kudos
Reply
2 Replies

1,734 Views
lisettelozano
NXP Employee
NXP Employee

Hello Larry,

The part marking corresponds to the MC34933EP.

Have a great day,

Paulina

0 Kudos
Reply

1,734 Views
lroth
Contributor I

Thank you very much!

Larry

0 Kudos
Reply