sja1105 traffic Forwarding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sja1105 traffic Forwarding

1,085 Views
haiyang
Contributor III

hi,

i use sja1105 to designe a switch ;

I want to implement a traffic forwarding function, all the traffic from port0 forwarding to port3,

What configuration should I do?

And i dont want  use vLAN ,is there a simple mirror function? 

best wish

Tags (1)
0 Kudos
Reply
1 Reply

1,065 Views
kaden
NXP Employee
NXP Employee

Hi @haiyang ,

i do have a few questions to provide an appropriate answer.

Which variant are you using? SJA1105PQRS or the older SJA1105TEL? We recommend using the SJA1105PQRS for new designs.

Which tools are you currently using to generate a configuration for the device? 

BR

Kevin  

 

0 Kudos
Reply