sd host controller driver for reading a linux image on a mx31 PDK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sd host controller driver for reading a linux image on a mx31 PDK board

1,879件の閲覧回数
josephb
Contributor I

Hi all,

I intend to boot linux off SD card on the mx31 3stack board. I hope this can be done by adding custom logic to U-boot/Redboot. But this would require a MMC/SD driver along with the host controller driver.

 

 

Is  there a readymade driver in Uboot/Redboot to do this.  Would this minimal driver support reading linux uImage off the SD Card. If then how

 

Thanks,

Joseph.

0 件の賞賛
返信
1 返信

1,056件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You need to have MX31 silicon version TO2.0.1 in order to boot from SD/MMC.

 

There is Redboot support for booting from SD/MMC on MX31 (TO2.0.1) on Redboot 200841 and later versions. There is also a pre-built image that can boot from from SD (mx31_3stack_redboot_mmc.bin).

 

You can use ATK to flash this image into SD card.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信