problem communicating NGX LPC4357 card with PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem communicating NGX LPC4357 card with PC

2,331件の閲覧回数
mednassim
Contributor I

 

My computer does not detect the NXP box (NGX technologies), even after having flashed the microcontroller with LPCXpresso.

0 件の賞賛
返信
5 返答(返信)

2,292件の閲覧回数
mednassim
Contributor I

to launch the simulation with canoe it is necessary that the PC communicates with the NXP card, 

also the red and green leds don't light up anymore and there is an overheating on the micro bga (NXP LPC4357)

 

0 件の賞賛
返信

2,284件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Sorry for the late response, Could you tell me if your device is enumerated in the device manager? if not maybe is something wrong with your code. When you say "having flashed the microcontroller" are you using the LPC-Link2? Because the board requires an external debug probe, to flash such as the LPC-Link2.

I suggest reviewing the information for the vendor because the board is similar to this LPC4330-Xplorer Board | NXP Semiconductors from NXP, both ports micro USB at the same time for powering the RJ45 and board.

Best regards,
Pavel

0 件の賞賛
返信

2,273件の閲覧回数
mednassim
Contributor I

Hello,

Could you tell me if your device is listed in the device manager?

 -No, "before damage yes".

When you say "having flashed the microcontroller" are you using the LPC-Link2?

 -Yes,

0 件の賞賛
返信

2,265件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I recommend using the ISP boot, in the application note explaining how to do it, chapter 1.3 Boot selection [Programming and Booting Images from External NOR FLASH on LPC553x/LPC55S3x (nxp.com)].

Best regards,
Pavel

0 件の賞賛
返信

2,319件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Could you elaborate further? I mean, What are the steps to reproduce your issue?

Best regards,
Pavel

-------------------------------------------

LPC4330-Xplorer Board | NXP Semiconductors

0 件の賞賛
返信