pn7161 ic without development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn7161 ic without development board

2,393件の閲覧回数
user_ahmed
Contributor II

hi 

i asking about if i buy pn7161 how can i adjust dpc

i see library related to Linux

so can i deal with it without Linux like arduino library 

because i don't see arduino library for it i found library to pn7150

 

thanks

0 件の賞賛
返信
5 返答(返信)

2,328件の閲覧回数
user_ahmed
Contributor II

Hi ,my question if there no Linux platform ?

how enable dpc ?

0 件の賞賛
返信

2,327件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

In fact, this AN13224 has clearly explained all the functions of DPC, including how to enable DPC on the different platforms, so what is your platform? We'll help you indicate how to enable DPC.

0 件の賞賛
返信

2,373件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

The DPC feature of PN7161 is the same as PN7160, so it's recommened that you can refer AN13224 (https://www.nxp.com/docs/en/application-note/AN13224.pdf) to adjust DPC. For Linux, the NFC Factory Test application can be used. Please check the AN13224 for the details.

0 件の賞賛
返信

2,357件の閲覧回数
user_ahmed
Contributor II

sorry i don't got you

you mean i can enable and disable it through test mode or Linux only ?

according to arduino or any mcu can i configure it?

0 件の賞賛
返信

2,339件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

Since PN7161 is running on a Linux platform on your site, it is recommended that you use the NFC Factory Test Application, which is not only enable or disable DPC, but also debugs and configures DPC, and writes the final data to EEPROM. So it is recommended that you read AN13224 carefully.

0 件の賞賛
返信