pn7161 ic without development board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pn7161 ic without development board

2,409 Views
user_ahmed
Contributor II

hi 

i asking about if i buy pn7161 how can i adjust dpc

i see library related to Linux

so can i deal with it without Linux like arduino library 

because i don't see arduino library for it i found library to pn7150

 

thanks

0 Kudos
Reply
5 Replies

2,344 Views
user_ahmed
Contributor II

Hi ,my question if there no Linux platform ?

how enable dpc ?

0 Kudos
Reply

2,343 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

In fact, this AN13224 has clearly explained all the functions of DPC, including how to enable DPC on the different platforms, so what is your platform? We'll help you indicate how to enable DPC.

0 Kudos
Reply

2,389 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

The DPC feature of PN7161 is the same as PN7160, so it's recommened that you can refer AN13224 (https://www.nxp.com/docs/en/application-note/AN13224.pdf) to adjust DPC. For Linux, the NFC Factory Test application can be used. Please check the AN13224 for the details.

0 Kudos
Reply

2,373 Views
user_ahmed
Contributor II

sorry i don't got you

you mean i can enable and disable it through test mode or Linux only ?

according to arduino or any mcu can i configure it?

0 Kudos
Reply

2,355 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

Since PN7161 is running on a Linux platform on your site, it is recommended that you use the NFC Factory Test Application, which is not only enable or disable DPC, but also debugs and configures DPC, and writes the final data to EEPROM. So it is recommended that you read AN13224 carefully.

0 Kudos
Reply