pn7161 ic without development board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pn7161 ic without development board

2,368 次查看
user_ahmed
Contributor II

hi 

i asking about if i buy pn7161 how can i adjust dpc

i see library related to Linux

so can i deal with it without Linux like arduino library 

because i don't see arduino library for it i found library to pn7150

 

thanks

0 项奖励
回复
5 回复数

2,303 次查看
user_ahmed
Contributor II

Hi ,my question if there no Linux platform ?

how enable dpc ?

0 项奖励
回复

2,302 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

In fact, this AN13224 has clearly explained all the functions of DPC, including how to enable DPC on the different platforms, so what is your platform? We'll help you indicate how to enable DPC.

0 项奖励
回复

2,348 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

The DPC feature of PN7161 is the same as PN7160, so it's recommened that you can refer AN13224 (https://www.nxp.com/docs/en/application-note/AN13224.pdf) to adjust DPC. For Linux, the NFC Factory Test application can be used. Please check the AN13224 for the details.

0 项奖励
回复

2,332 次查看
user_ahmed
Contributor II

sorry i don't got you

you mean i can enable and disable it through test mode or Linux only ?

according to arduino or any mcu can i configure it?

0 项奖励
回复

2,314 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

Since PN7161 is running on a Linux platform on your site, it is recommended that you use the NFC Factory Test Application, which is not only enable or disable DPC, but also debugs and configures DPC, and writes the final data to EEPROM. So it is recommended that you read AN13224 carefully.

0 项奖励
回复