pcf85263a offset adjust

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pcf85263a offset adjust

1,226件の閲覧回数
pivent
Contributor I

Hi,

I am using  PCF85263A RTC chipset in my product.

It gets faster every day. So, I want to adjust offset register. (24h Offset OFFSET[7:0])

I don't under stand 2 point.

1. I want to slow RTC .   Now RTC get faster every day. Then adding or subtracting  clock ? 

-----------------

The correction is made by adding or subtracting clock correction pulses, thereby changing
the period of a single second but not by changing the oscillator frequency.
 

-------------

2.  , Would you explain more about below?   once every four hours ?  once per minute ?

 Correction when OFFM = 0  

The correction is triggered once every four hours and then correction pulses are applied
once per minute until the programmed correction values have been implemented

Best Regards

Jae Won

0 件の賞賛
返信
1 返信

1,122件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please see comment for your questions:

1: A positive value written to the Offset Register will cause the RTC device to run slower and a negative value written to the Offset Register will cause the RTC device to run faster.

2:For the example you can refer to datasheet page37 Figure19

0 件の賞賛
返信