open SDA 1.21

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

open SDA 1.21

1,150 次查看
haidong_zhang
Contributor I

Dear,

I bought a S32K142_EVB for study, but from yesterday the debugger of IDE can't connect to the board shows P&E connection error, I tried to update the openSDA of the board with S32K144 SDA but failed.

then I searched on the NXP  comment,  some where have "MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA" but I can't found it.

if it is possible I need "MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA" or more suitable SDA for my board.

thank you!

标记 (1)
0 项奖励
回复
1 回复

1,093 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Haidong Zhang 

The OpenSDA firmware for S32K142_evb can be downloaded from the P&EMicro page:

PEmicro | Experts in Embedded tools for Flash Programming and Development 

In Firmware Apps You will find a zip package with the .SDA

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 项奖励
回复