on chip PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

on chip PWM

2,671 Views
Engineer_xxx
Contributor II

Hello team 

Im trying to select PWM GPIO from below picture, which one will be good fit please? also if you can explain the picture please will be nice. 
Thanks

Engineer_xxx_0-1731775135903.png

 

0 Kudos
Reply
5 Replies

2,571 Views
mayliu1
NXP Employee
NXP Employee

Dear @Engineer_xxx ,

 

Thank you so much for your interest in our products and for using our community.

Question:  select PWM GPIO in PWM1.

Answer: It depends on your needs, PWM outputs that can operate as complementary pairs or independent channels.

If you want PWM outputs operate  as an independent channel , you can select one from A0~A3, B0~B3(Total 8 channels).

I suggest you can refer SDK demo "evkbmimxrt1170_pwm_cm7". I think it is very useful for reference.

mayliu1_1-1732014162892.png

Question: also if you can explain the picture please will be nice. 

Answer:  I suggest you can refer chapter 73.4 External signals in MIMXRT1170RM, It describes very detail.

https://www.nxp.com/webapp/Download?colCode=IMXRT1170RM

mayliu1_2-1732014928438.png

mayliu1_3-1732014944220.png

 

Wish it helps you.
If you still have question about it, please kindly let me know.

 

Best Regards

mayliu

2,563 Views
Engineer_xxx
Contributor II
BIG THANKS BROTHER
0 Kudos
Reply

2,561 Views
mayliu1
NXP Employee
NXP Employee

Hi @Engineer_xxx 

Dear Engineer_xxx, If your question is solved, please tell me to close this case, and help me set this as solution, thank you very much.

 

Wish you a nice day!

 

Best Regards

mayliu

0 Kudos
Reply

2,604 Views
LinaHou
NXP TechSupport
NXP TechSupport
Thanks for contacting us.
 
Unfortunately, I am not able to determine your request based on the information provided
 
Would you pls provide which NXP product are you using now?
 
Then, I could assign your request to our responsible engineer team.
they will you a more accurate and Professional support.
 
Look forward to your reply.
 
Thank you and have a nice day.
0 Kudos
Reply

2,601 Views
Engineer_xxx
Contributor II
Hello LinaHou
Thanks for your response, its MIMXRT1171.
Thanks
0 Kudos
Reply