nmcli command is not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nmcli command is not working.

1,601 Views
jun_1
Contributor IV

I'm trying to execute "nmcli device wifi connect ssid password" command to measure WiFi access point connection time, but it seems that nmcli command is not implemented in i.MX Yocto.
Could you tell me an alternative command or a way to use nmcli command on i.MX Yocto?

Environment
i.MX 8M Mini EVKB
OS:LF_v6.6.23-2.0.0_images_IMX8MMEVK.zip

0 Kudos
Reply
1 Reply

1,583 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello, @jun_1 

 

You can look the Linux i.MX User's guide on chapter 11.1 Connectivity for Bluetooth wireless technology and Wi-Fi

There is explained how you can use the connmanctl to WIFI operations.

 

Best regards,

Salas.

0 Kudos
Reply