mpc8313uboot nor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,465件の閲覧回数
leilei987
Contributor II

hi
i project use mpc8313
uboot printf


U-Boot 1.1.6-gacb2702c-dirty (Apr 15 2021 - 14:24:48) MPC83XX
Board LF7511
CPU: MPC8313, Rev: 21 at 333.333 MHz
INFO: Initializing IOMEM for regset 0
INFO: reset phy for M88E1340 card
DRAM: 256 MB
FLASH: 64 MB
NAND: 256 MB
Using default environment
In: serial
Out: serial
Err: serial
Net: ....TSEC1: PHY is Marvell 88E1340 (1410dc0)
....TSEC2: PHY is Marvell 88E1340 (1410dc0)
TSEC1 [PRIME], TSEC2
Boot in 3 seconds
=> ......


#define CFG_BR0_BASE 0xe8000000 /* u-boot presumes it is the address needed to */
#define CFG_FLASH_CFI /* use the Common Flash Interface */
#define CFG_FLASH_CFI_DRIVER /* use the CFI driver */
#define CFG_FLASH_BASE CFG_BR0_BASE /* start of FLASH */
#define CFG_FLASH_SIZE 64 /* flash size in MB */
#define CFG_FLASH_EMPTY_INFO /* display empty sectors */
#define CFG_FLASH_USE_BUFFER_WRITE /* buffer up multiple bytes */
#define CFG_BR0_PRELIM 0xe8001001
#define CFG_OR0_PRELIM 0xfc006ff7
#define CFG_LBLAWBAR0_PRELIM CFG_FLASH_BASE /* window base at flash base */
#define CFG_LBLAWAR0_PRELIM 0x80000019 /* 64 MB window size */
#define CFG_MAX_FLASH_BANKS 1 /* number of banks */
#define CFG_MAX_FLASH_SECT 512 /* sectors per device */

 

# define CFG_BR1_BASE 0xD0000000
# define CFG_NAND_BASE CFG_BR1_BASE
# define CFG_LBLAWBAR1_PRELIM CFG_BR1_BASE
# define CFG_LBLAWAR1_PRELIM 0x8000001b
# define CFG_BR1_PRELIM ( CFG_BR1_BASE | (2<<BR_DECC_SHIFT) | BR_MS_FCM | BR_PS_8 | BR_V )
# define CFG_OR1_PRELIM ( 0xF0000000 | OR_FCM_PGS | OR_FCM_CSCT | OR_FCM_CST | OR_FCM_CHT | OR_FCM_SCY_4 | OR_FCM_TRLX | OR_FCM_EHTR )

The code above is my br0 or0 br1 or1 config
cs0 is link S29GL512T nor flash
cs1 is link MT29F2G08ABAEA nand falsh

I use bdi2000 load uboot.bin to ddr
uart input as follow cmd :

erase e8000000 +0x100000

tftp 0x100000 u-boot.bin

cp.b 0x100000 0xe8000000 $filesize

cmp.b 0x100000 0xe8000000 $filesize

burn the uboot.bin to norflash 0 space

i want to uboot self-starting nor flash because old version is self-starting nand flash

first
the hardware modified:
1 CFG_RESET_SOURCE[0:3]=TSEC2_TXD[3:0] 0000
2 cs0 is link nor faslh

 

second

uboot code modyfi front
CFG_HRCW_HIGH hrcw config

BMS is 0b ROMLOC 011b RLEXT 00b

but uart no printf? ? ?wait 10s??The serial port is not printed out either
how about ,
rcw br or?
Is there anything else that needs to be revised and confirmed

0 件の賞賛
返信
1 解決策
4,424件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please compile u-boot with configs/MPC8313ERDB_33_defconfig or MPC8313ERDB_66_defconfig.

Please modify your u-boot configuration based on include/configs/MPC8313ERDB.h.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,449件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Did you do your porting based on MPC8313ERDB?

Did you modify include/configs/MPC8313ERDB.h? Would you please provide your header file in include/configs/?

Please check whether SYS_TEXT_BASE is defined correctly, please refer to the following.

#ifndef CONFIG_SYS_TEXT_BASE
#define CONFIG_SYS_TEXT_BASE 0xe8000000
#endif

0 件の賞賛
返信
4,441件の閲覧回数
leilei987
Contributor II

hi 

YIPING

i use uboot version is 1.1.6

this version have a little old

only in  my private compile  Script have:

ifndef TEXT_BASE
TEXT_BASE = 0x1000000
endif

 

and private boards .h   as follow

/*
 * Copyright (C) Freescale Semiconductor, Inc. 2006.
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
 * MA 02111-1307 USA
 *
 * History
 * 20061201: Wilson Lo ([email protected])
 *           Initialized 
 *
 * 20061210: Tanya Jiang ([email protected])
 *           Code Cleanup
 *
 */
 
#ifndef __CONFIG_H
#define __CONFIG_H
 
#undef DEBUG
#ifdef CONFIG_TEST
#warning WARNING WARNING: TEST CONFIGURATION ENABLED
#endif
 
#define CONFIG_JFFS2_SUMMARY
//#define CONFIG_SYS_JFFS2_SORT_FRAGMENTS
 
 
/*
 * High Level Configuration Options
 */
#define CONFIG_E300 1
#define CONFIG_MPC83XX 1
#define CONFIG_MPC8313 1
#define CONFIG_S8313         1
 
#if 0
#define CONFIG_83XX_CLKIN 33333333 /* in Hz */
#define CONFIG_SYS_CLK_FREQ 33333333    
#define CONFIG_83XX_PCICLK      33333333
#endif
 
#define CONFIG_83XX_CLKIN 33333333 /* in Hz */
#define CONFIG_SYS_CLK_FREQ 33333333    
#define CONFIG_83XX_PCICLK      33333333
 
#define CFG_SCCR ( SCCR_RES              \
| SCCR_TSEC1CM_1\
| SCCR_TSEC1ON\
| SCCR_TSEC2ON\
| SCCR_ENCCM_3\
| SCCR_USBCM_3\
| SCCR_PCICM)
 
#define CONFIG_BOARD_EARLY_INIT_F
#undef  CONFIG_BOARD_EARLY_INIT_F
 
#define CONFIG_BOARD_EARLY_INIT_R
#undef  CONFIG_BOARD_EARLY_INIT_R
 
#define CFG_IMMR 0xE0000000
 
#define CFG_SPI_MODE            (CFG_IMMR+0x20)
#define CFG_SPIE                (CFG_IMMR+0x24)
#define CFG_SPIM                (CFG_IMMR+0x28)
#define CFG_SPICOM              (CFG_IMMR+0x2C)             
#define CFG_SPITD               (CFG_IMMR+0x30)
#define CFG_SPIRD               (CFG_IMMR+0x34)
 
/* used by memory cmd */
 
#define CFG_ALT_MEMTEST                 /* use slow test */
#define CFG_MEMTEST_START (  1 * 1024 * 1024)
#define CFG_MEMTEST_END   ( 16 * 1024 * 1024)
 
/*
 * DDR Setup
 */
 
#undef CONFIG_SPD_EEPROM
 
#define CFG_DDR_BASE 0x00000000
#define CFG_SDRAM_BASE CFG_DDR_BASE
#define CFG_DDR_SDRAM_BASE CFG_DDR_BASE
 
#undef  CONFIG_DDR_2T_TIMING
 
#ifndef CSCONFIG_BA_2
#  define CSCONFIG_BA_2 0
#endif
 
#ifndef CSCONFIG_BA_3
#  define CSCONFIG_BA_3 0x4000
#endif
 
#define CFG_DDR_SIZE 256 /* MB */
#define CFG_DDR_CONFIG         ( CSCONFIG_EN | CSCONFIG_AP | CSCONFIG_ODT_RD_1 | CSCONFIG_ODT_WR_1 \
  | CSCONFIG_BA_3 \
  | CSCONFIG_ROW_BIT_13 | CSCONFIG_COL_BIT_10 )
 
#define CFG_DDRCDR ( DDRCDR_EN \
| DDRCDR_PZ_NOMZ \
| DDRCDR_NZ_NOMZ \
| DDRCDR_M_ODR )
 
#define CFG_DDR_CLK_CNTL DDR_SDRAM_CLK_CNTL_CLK_ADJUST_05
 
#define CFG_DDR_TIMING_3 0x00000000
 
#define CFG_DDR_TIMING_0 ( ( 0 << TIMING_CFG0_RWT_SHIFT ) \
| ( 0 << TIMING_CFG0_WRT_SHIFT ) \
| ( 0 << TIMING_CFG0_RRT_SHIFT ) \
| ( 0 << TIMING_CFG0_WWT_SHIFT ) \
| ( 3 << TIMING_CFG0_ACT_PD_EXIT_SHIFT ) \
| ( 3 << TIMING_CFG0_PRE_PD_EXIT_SHIFT ) \
| (10 << TIMING_CFG0_ODT_PD_EXIT_SHIFT ) \
| ( 3 << TIMING_CFG0_MRS_CYC_SHIFT ) )
 
#define CFG_DDR_TIMING_1 ( ( 6 << TIMING_CFG1_PRETOACT_SHIFT ) \
| ( 0 << TIMING_CFG1_ACTTOPRE_SHIFT ) \
| ( 6 << TIMING_CFG1_ACTTORW_SHIFT ) \
| ( 5 << TIMING_CFG1_CASLAT_SHIFT ) \
| (15 << TIMING_CFG1_REFREC_SHIFT ) \
| ( 7 << TIMING_CFG1_WRREC_SHIFT ) \
| ( 5 << TIMING_CFG1_ACTTOACT_SHIFT ) \
| ( 4 << TIMING_CFG1_WRTORD_SHIFT ) )
 
#define CFG_DDR_TIMING_2 ( ( 0 << TIMING_CFG2_ADD_LAT_SHIFT ) \
| (31 << TIMING_CFG2_CPO_SHIFT ) \
| ( 2 << TIMING_CFG2_WR_LAT_DELAY_SHIFT ) \
| ( 2 << TIMING_CFG2_RD_TO_PRE_SHIFT ) \
| ( 2 << TIMING_CFG2_WR_DATA_DELAY_SHIFT ) \
| ( 3 << TIMING_CFG2_CKE_PLS_SHIFT ) \
| (10 << TIMING_CFG2_FOUR_ACT_SHIFT) )
 
#define CFG_DDR_INTERVAL ( ( 800 << SDRAM_INTERVAL_REFINT_SHIFT ) \
| ( 100 << SDRAM_INTERVAL_BSTOPRE_SHIFT ) )
 
#if defined(CONFIG_DDR_2T_TIMING)
 
# define CFG_SDRAM_CFG ( SDRAM_CFG_SREN \
| 3 << SDRAM_CFG_SDRAM_TYPE_SHIFT \
| SDRAM_CFG_2T_EN \
| SDRAM_CFG_DBW_32 )
 
#else
 
# define CFG_SDRAM_CFG ( SDRAM_CFG_SREN \
| 3 << SDRAM_CFG_SDRAM_TYPE_SHIFT \
| SDRAM_CFG_DBW_32 )
#endif
 
#define CFG_SDRAM_CFG2 0x00601000;
 
#define CFG_DDR_MODE ( ( 0x4440 << SDRAM_MODE_ESD_SHIFT ) \
| ( 0x0232 << SDRAM_MODE_SD_SHIFT ) )
 
#define CFG_DDR_MODE_2 0x8000C000;
 
/* 
 * Before the NAND stage 0 boot loader relocates U-BOOT
 * RAM is tested - but only a small amount since cache is turned off
 */
#define CONFIG_NAND_DDR_TEST_START0  (  0 * 1024 * 1024 )
#define CONFIG_NAND_DDR_TEST_END0    (  2 * 1024 * 1024 )
 
#define CONFIG_NAND_DDR_TEST_START1  (( CFG_DDR_SIZE - 2 ) * 1024 * 1024)
#define CONFIG_NAND_DDR_TEST_END1    (( CFG_DDR_SIZE     ) * 1024 * 1024)
 
#define CONFIG_NAND_DDR_TEST_LIST  {                                    \
    CONFIG_NAND_DDR_TEST_START0, CONFIG_NAND_DDR_TEST_END0, \
    CONFIG_NAND_DDR_TEST_START1, CONFIG_NAND_DDR_TEST_END1         \
      }
 
/*
 * Once U-BOOT is loaded it can test RAM, however it must avoid certain address
 * ranges ....
 */
 
#define CONFIG_U_BOOT_DDR_TEST_START0  (              2  * 1024 * 1024)
#define CONFIG_U_BOOT_DDR_TEST_END0    ((CFG_DDR_SIZE-2) * 1024 * 1024)
 
#define CONFIG_U_BOOT_DDR_TEST_LIST    {                                \
    CONFIG_U_BOOT_DDR_TEST_START0, CONFIG_U_BOOT_DDR_TEST_END0 \
      }
 
/*
 * NO FLASH
 */
#if 0  
#define CFG_NO_FLASH
#endif
#define ADD_FLASH_CMD          (0)
 
 
#define CFG_INIT_RAM_LOCK 1
#if 1
#define CFG_INIT_RAM_ADDR 0xFD000000 /* Initial RAM address */
#endif
#define CFG_INIT_RAM_END 0x1000 /* End of used area in RAM*/
 
#define CFG_GBL_DATA_SIZE 0x100 /* num bytes initial data */
#define CFG_GBL_DATA_OFFSET (CFG_INIT_RAM_END - CFG_GBL_DATA_SIZE)
#define CFG_INIT_SP_OFFSET CFG_GBL_DATA_OFFSET
 
/*
 * Monitor
 */
#define CFG_MONITOR_BASE TEXT_BASE       /* ((CFG_DDR_SIZE-1) * 0x100000) */ 
 
#define CFG_MONITOR_LEN ( 384 * 1024) /* Reserved for Mon */
#define CFG_MALLOC_LEN ( 512 * 1024) /* Reserved for malloc */
//#define CFG_GBL_DATA_SIZE       ( 128 * 1024)   /* Global data */
#if 0
#if (CFG_MONITOR_BASE < CFG_FLASH_BASE) && !defined(CONFIG_NAND_U_BOOT)
#define CFG_RAMBOOT
#else
#undef  CFG_RAMBOOT
#endif
#endif
/*
 * This is a special case: the startup code maps LAW1 based on
 * the value of CFG_FLASH_BASE and CFG_FLASH_SIZE.
 *
 * This allows us to fool the system into thinking we are mapped
 * when we are not ( FCM failed )
 */
#if 0
#define CFG_FLASH_BASE         CFG_MONITOR_BASE      
#define CFG_FLASH_SIZE         CFG_MONITOR_LEN
#endif
/*
 * Local Bus LCRR and LBCR regs (0 is boot, 1..6)
 */
 
#define CFG_LCRR         LCRR_EADC_1 | LCRR_CLKDIV_4
#define CFG_LBC_LBCR        (0x00040000 | (0xFF << LBCR_BMT_SHIFT) | 0xF)
#define CFG_LBC_MRTPR         0x20000000
 
/* Default values to make it easy to add/modify CS's for debugging */
#define CFG_BR_DEFAULT          0x00000801       /* 8b GPCM */
#define CFG_BR_DEFAULT_16       0x00001001       /* 16b GPCM */
#define CFG_OR_DEFAULT          0xFFFF8104       /* 32k UPM */
#define CFG_OR_DEFAULT_1M       0xFFF00104       /* 1m UPM */
#define CFG_LBLAWAR_DEFAULT     0x8000000E       /* 32k     */
#define CFG_LBLAWAR_DEFAULT_1M  0x80000013       /* 1m      */
 
/* CFG_BRX_BASE needed by s8313.c */
 
#ifdef CONFIG_NAND_SPL
 
#  define CFG_NAND_BASE         0xfff00000    /* not what you think!                           */
                                              /* load address for stage0 code, 0xfff00000 based*/
                                              /* on BM bit ( 0x0 or 0xfff... )                 */
#else
 
 
#if 0
/* local bus CS 0 - NAND flash */
 
#  define CFG_BR0_BASE          0xe8000000    /* u-b
oot presumes it is the address needed to   */
                                              /* access the chip ( ale ... )                   */
 
#  define CFG_NAND_BASE         CFG_BR0_BASE  /* value used by u-boot to access chip           */
 
#  define CFG_LBLAWBAR0_PRELIM CFG_BR0_BASE
#  define CFG_LBLAWAR0_PRELIM 0x8000000E 
#  define CFG_BR0_PRELIM ( CFG_BR0_BASE | (2<<BR_DECC_SHIFT) | BR_PS_8 | BR_MS_FCM | BR_V )
#  define CFG_OR0_PRELIM  ( 0xFFFF8000 | OR_FCM_PGS | OR_FCM_CSCT | OR_FCM_CST | OR_FCM_CHT | OR_FCM_SCY_4 | OR_FCM_TRLX | OR_FCM_EHTR )
#endif
#define CFG_BR0_BASE          0xe8000000    /* u-boot presumes it is the address needed to   */
#define CFG_FLASH_CFI /* use the Common Flash Interface */
#define CFG_FLASH_CFI_DRIVER /* use the CFI driver */
#define CFG_FLASH_BASE CFG_BR0_BASE /* start of FLASH   */
#define CFG_FLASH_SIZE 64 /* flash size in MB */
#define CFG_FLASH_EMPTY_INFO /* display empty sectors */
#define CFG_FLASH_USE_BUFFER_WRITE /* buffer up multiple bytes */
 
 
#define CFG_BR0_PRELIM          0xe8001001
#if 0
#define CFG_BR0_PRELIM (CFG_FLASH_BASE |    /* flash Base address */ \
(2 << BR_PS_SHIFT) | /* 16 bit port size */ \
BR_V)     /* valid */
 
#define CFG_FLASH_OR_PRELIM ( 0xFF000000         /* 16 MByte */ \
| OR_GPCM_XACS \
| OR_GPCM_SCY_9 \
| OR_GPCM_EHTR \
| OR_GPCM_EAD )
/* 0xFF006FF7TODO SLOW 16 MB flash size */
#define CFG_MAX_FLASH_SECT 512 /* sectors per device */
#endif
#define CFG_OR0_PRELIM      0xfc006993
#define CFG_LBLAWBAR0_PRELIM CFG_FLASH_BASE /* window base at flash base */
#define CFG_LBLAWAR0_PRELIM 0x80000019 /* 64 MB window size */
#define CFG_MAX_FLASH_BANKS 1 /* number of banks */
#define CFG_MAX_FLASH_SECT 512 /* sectors per device */
 
 
 
/* local bus CS 1  */
#if 0
#  define CFG_BR1_BASE         0xe9000000
#  define CFG_LBLAWBAR1_PRELIM CFG_BR1_BASE
#  define CFG_NAND_BASE         CFG_BR1_BASE 
#  define CFG_LBLAWAR1_PRELIM CFG_LBLAWAR_DEFAULT
#  define CFG_BR1_PRELIM CFG_BR1_BASE | CFG_BR_DEFAULT | BR_MS_UPMA
#  define CFG_OR1_PRELIM CFG_OR_DEFAULT
#else
 
 
#  define CFG_BR1_BASE         0xD0000000
#  define CFG_NAND_BASE         CFG_BR1_BASE 
#  define CFG_LBLAWBAR1_PRELIM CFG_BR1_BASE
#  define CFG_LBLAWAR1_PRELIM 0x8000001b
#if 0
#  define CFG_BR1_PRELIM ( CFG_BR1_BASE | (2<<BR_DECC_SHIFT) | BR_PS_8 | BR_MS_FCM | BR_V )
#  define CFG_OR1_PRELIM ( 0xFFFF8000 | OR_FCM_PGS | OR_FCM_CSCT | OR_FCM_CST | OR_FCM_CHT | OR_FCM_SCY_4 | OR_FCM_TRLX | OR_FCM_EHTR )
#endif
#  define CFG_BR1_PRELIM ( CFG_BR1_BASE  | (2<<BR_DECC_SHIFT) | BR_MS_FCM | BR_PS_8 | BR_V )
#  define CFG_OR1_PRELIM ( 0xF0000000    | OR_FCM_PGS | OR_FCM_CSCT | OR_FCM_CST | OR_FCM_CHT | OR_FCM_SCY_4 | OR_FCM_TRLX | OR_FCM_EHTR )
#endif
 
 
 
/* local bus CS 2  */
#  define CFG_BR2_BASE         0xed000000
#  define CFG_LBLAWBAR2_PRELIM CFG_BR2_BASE
#  define CFG_OR2_PRELIM CFG_OR_DEFAULT
#  define CFG_LBLAWAR2_PRELIM CFG_LBLAWAR_DEFAULT
 
#if defined(CONFIG_CPU_DAUGHTER_8313) || defined(CONFIG_TC1000_8313) || defined(CONFIG_SCRDB_8313) || defined(CONFIG_FRISER_8313) || defined(CONFIG_PTPIN) || defined(CONFIG_FIBER) || defined(CONFIG_LF7520) || defined(CONFIG_LF7550)|| defined(CONFIG_LF7511)
#  define CFG_BR2_PRELIM CFG_BR2_BASE | CFG_BR_DEFAULT | BR_MS_UPMB
#  define CFG_S8313_UPMB 1
#else
#define CFG_BR2_PRELIM CFG_BR2_BASE | CFG_BR_DEFAULT | BR_MS_UPMA
#endif
 
 
 
/* local bus CS 3  */
#if defined(CONFIG_SM2000_PTP_OUT)
#define CFG_BR3_BASE 0xec000000
#define CFG_LBLAWBAR3_PRELIM CFG_BR3_BASE
#define CFG_OR3_PRELIM CFG_OR_DEFAULT
#define CFG_LBLAWAR3_PRELIM CFG_LBLAWAR_DEFAULT
#define CFG_BR3_PRELIM CFG_BR3_BASE | CFG_BR_DEFAULT | BR_MS_UPMA
 
#else
#  define CFG_BR3_BASE         0xfe000000
#  define CFG_LBLAWBAR3_PRELIM CFG_BR3_BASE
#  define CFG_LBLAWAR3_PRELIM CFG_LBLAWAR_DEFAULT
#  define CFG_BR3_PRELIM CFG_BR3_BASE | CFG_BR_DEFAULT | BR_MS_UPMA
#  define CFG_OR3_PRELIM CFG_OR_DEFAULT
#endif
#if 0  /*if close follow code  the serial no printf why? ll to do*/
/* local bus CS 4  */
#  define CFG_BR4_BASE         0xec000000
#  define CFG_LBLAWBAR4_PRELIM CFG_BR4_BASE
#  define CFG_LBLAWAR4_PRELIM CFG_LBLAWAR_DEFAULT
#  define CFG_BR4_PRELIM CFG_BR4_BASE | CFG_BR_DEFAULT | BR_MS_UPMA
#  define CFG_OR4_PRELIM CFG_OR_DEFAULT
#endif
 
 
 
#endif /* NAND_SPL */
 
/*
 * NAND Boot Configuration
 */
 
# define CFG_MAX_NAND_DEVICE 1
# define NAND_MAX_CHIPS         1
 
# define CONFIG_MTD_NAND_VERIFY_WRITE
 
# define CFG_NAND_BOOT_QUIET
# undef  CFG_NAND_BOOT_QUIET
 
/* 
 * 1) This must match u-boot-nand.lds
 *
 * #ifdef CONFIG_NAND_SPL
 *    use CFG_NAND_BASE as relocation address
 * #else
 *    use CFG_MONITOR_BASE as relocation address ( usually TEXT )
 *
 */
#define CFG_NAND_RELOC (0x4000)
 
#define CFG_NAND_PAGE_SIZE (2048)
#define CFG_NAND_BLOCK_SIZE (CFG_NAND_PAGE_SIZE*64)
 
#define CFG_NAND_FMR ((12 << FMR_CWTO_SHIFT) | (1 << FMR_AL_SHIFT) | FMR_ECCM )
 
#define CFG_NAND_BAD_BLOCK_POS (0)
 
#define CFG_NAND_U_BOOT_SIZE (384 << 10)
 
/* put it into top 1 mb */
#define CFG_NAND_U_BOOT_DST TEXT_BASE
#define CFG_NAND_U_BOOT_START (CFG_NAND_U_BOOT_DST + 0x120)
 
/* This must be undefined for CFG_RESET_ADDRESS to work */
#undef MPC83xx_RESET
 
#define CFG_RESET_ADDRESS       CFG_NAND_U_BOOT_START
 
/* 
 * pass open firmware flat tree 
 */
#define CONFIG_OF_FLAT_TREE 1
#define CONFIG_OF_BOARD_SETUP 1
#define OF_FLAT_TREE_MAX_SIZE 8192
 
#define OF_CPU "PowerPC,8313@0"
#define OF_SOC "soc8313@e0000000"
#define OF_TBCLK (bd->bi_busfreq / 4)
#define OF_STDOUT_PATH "/soc8313@e0000000/serial@4500"
 
/*
 * Serial Port
 */
#define CONFIG_CONS_INDEX 1
#undef  CONFIG_SERIAL_SOFTWARE_FIFO
 
#define CFG_NS16550
#define CFG_NS16550_SERIAL
#define CFG_NS16550_REG_SIZE 1
#define CFG_NS16550_CLK get_bus_freq(0)
 
#define CFG_BAUDRATE_TABLE \
{300, 600, 1200, 2400, 4800, 9600, 19200, 38400,115200}
 
#define CFG_NS16550_COM1 (CFG_IMMR+0x4500)
#define CFG_NS16550_COM2 (CFG_IMMR+0x4600)
#define CONFIG_CMDLINE_EDITING 1 /* add command line history  modify by ll 20210406*/
 
 
/* 
 * I2C 
 */
#undef CONFIG_HARD_I2C
#undef CONFIG_SOFT_I2C
 
#define CONFIG_FSL_I2C
#define CONFIG_I2C_MULTI_BUS
#define CONFIG_I2C_CMD_TREE
#define CFG_I2C_SPEED 400000
#define CFG_I2C_SLAVE 0x7F
#define CFG_I2C_NOPROBES {0x69}
#define CFG_I2C_OFFSET 0x3000
#define CFG_I2C2_OFFSET 0x3100
 
/*
* defined for SGMII config lsk 2018-4-8
*/
#define CONFIG_MPC8313_SGMII 1
 
/* TSEC */
#define CFG_TSEC1_OFFSET 0x24000
#define CFG_TSEC1 (CFG_IMMR+CFG_TSEC1_OFFSET)
 
#define CFG_TSEC2_OFFSET 0x25000
#define CFG_TSEC2 (CFG_IMMR+CFG_TSEC2_OFFSET)
 
/*
 * TSEC configuration
 */
#define CONFIG_TSEC_ENET
 
#if defined(CONFIG_TSEC_ENET)
#if defined(CONFIG_SM2000_PTP_OUT)
# define CONFIG_MPC83XX_TSEC2 1
# define CONFIG_MPC83XX_TSEC2_NAME "TSEC2"
#elif defined(CONFIG_SM2000_NTP_OUT)
# define CONFIG_MPC83XX_TSEC2 1
# define CONFIG_MPC83XX_TSEC2_NAME "TSEC2"
#else
# define CONFIG_MPC83XX_TSEC1 1
# define CONFIG_MPC83XX_TSEC1_NAME "TSEC1"
# define CONFIG_MPC83XX_TSEC2 1
# define CONFIG_MPC83XX_TSEC2_NAME "TSEC2"
#endif
 
#if defined(CONFIG_SM1000)
#define TSEC1_PHY_ADDR 3
#define TSEC2_PHY_ADDR 0
#elif defined(CONFIG_SM2000_CC)
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#elif defined(CONFIG_SM2000_PTP_OUT) || defined(CONFIG_SM2000_NTP_OUT)
#define TSEC2_PHY_ADDR 2
#elif defined(CONFIG_SM2000_NTP_OUT)
#define TSEC2_PHY_ADDR 2
#elif defined(CONFIG_MOC700)
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#elif defined(CONFIG_LF7560)
#define TSEC1_PHY_ADDR 2
#define TSEC2_PHY_ADDR 3
#elif defined(CONFIG_LF7500)
#define TSEC1_PHY_ADDR 2
#define TSEC2_PHY_ADDR 3
#elif defined(CONFIG_LF7520)
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#elif defined(CONFIG_LF7550)
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#elif defined(CONFIG_LF7511)
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#else
#define TSEC1_PHY_ADDR 0
#define TSEC2_PHY_ADDR 1
#endif
 
# define TSEC1_PHYIDX 0
# define TSEC2_PHYIDX 0
 
#endif /* CONFIG_TSEC_ENET */
 
/*
 * Environment
 */
#if 0
#define CFG_ENV_IS_NOWHERE 1 /* Store ENV in memory only */
#define CFG_ENV_ADDR (CFG_MONITOR_BASE - 0x2000)
#define CFG_ENV_SIZE 0x2000
#endif
#if defined(CONFIG_NAND_U_BOOT)
#define CFG_ENV_IS_IN_NAND1
#define CFG_ENV_SIZECFG_NAND_BLOCK_SIZE
#define CFG_ENV_OFFSET((512<<10) - (CFG_NAND_BLOCK_SIZE<<1))
#elif !defined(CFG_RAMBOOT)
#define CFG_ENV_IS_IN_FLASH1
#define CFG_ENV_ADDR(CFG_MONITOR_BASE + 0x50000)
#define CFG_ENV_SECT_SIZE0x20000/* 128K(one sector) for env */
#define CFG_ENV_SIZE0x20000
 
/* Address and size of Redundant Environment Sector */
#else
#define CFG_ENV_IS_NOWHERE1/* Store ENV in memory only */
#define CFG_ENV_ADDR(CFG_MONITOR_BASE - 0x2000)
#define CFG_ENV_SIZE0x2000
#endif
 
#define CONFIG_LOADS_ECHO 1 /* echo on for serial download */
#define CFG_LOADS_BAUD_CHANGE 1 /* allow baudrate change */
 
#define CFG_BASE_COMMANDS ( CONFIG_CMD_DFL \
| CFG_CMD_PING\
| CFG_CMD_NET           \
| CFG_CMD_MII\
| CFG_CMD_BOOTM         \
| CFG_CMD_PCI           \
| CFG_CMD_JFFS2        \
| CFG_CMD_NAND        \
                                | ADD_FLASH_CMD         \
| CFG_CMD_FLASH\
)
 
#if 0
#define CFG_RAMBOOT_COMMANDS ( CFG_BASE_COMMANDS & ~( CFG_CMD_ENV | CFG_CMD_LOADS | CFG_CMD_FLASH | CFG_CMD_IMLS))
#endif
#define CFG_RAMBOOT_COMMANDS ( CFG_BASE_COMMANDS & ~( CFG_CMD_ENV | CFG_CMD_LOADS  | CFG_CMD_IMLS))
 
#define CONFIG_COMMANDS         ( CFG_RAMBOOT_COMMANDS )
 
#include <cmd_confdefs.h>
 
/*
 * WATCHDOG MADDNESS
 */
 
/* 
 * watchdog is not implemented for MPC83xx even though
 * bits and pieces are present.
 *
 * Routine 'watchdog_reset' must be defined in BSP
 */
#undef CONFIG_WATCHDOG
 
/* 
 * HW watchdog is not implemented for MPC83xx even 
 * though bits and pieces are present.
 *
 * Routine 'hw_watchdog_reset' must be defined in BSP
 */
#undef CONFIG_HW_WATCHDOG
 
/*
 * This is used by s8313.c and by the u-boot code
 *
 */
#define CFG_WATCHDOG_VALUE 0xFFFFFFC3
 
/*
 * Miscellaneous configurable options
 */
#define CFG_LONGHELP
 
#define CFG_PROMPT "=> "
 
/* Use the HUSH parser */
#define CFG_HUSH_PARSER
#ifdef  CFG_HUSH_PARSER
# define CFG_PROMPT_HUSH_PS2 "=> "
#endif
 
/* console buffer size */
#define CFG_CBSIZE 1024
 
#define CFG_PBSIZE      (CFG_CBSIZE+sizeof(CFG_PROMPT)+16) /* Print Buffer Size */
#define CFG_MAXARGS 16                    /* max number of command args */
#define CFG_BARGSIZE CFG_CBSIZE                    /* Boot Argument Buffer Size */
#define CFG_HZ 1000                    /* decrementer freq: 1ms ticks */
 
/*
 * For booting Linux, the board info and command line data
 * have to be in the first 8 MB of memory, since this is
 * the maximum mapped by the Linux kernel during initialization.
 *
 * well not exactly ... values up to 254>>20 work...
 *
 */
#define CFG_BOOTMAPSZ (254<<20)
 
/* Cache Configuration */
 
#define CFG_DCACHE_SIZE 16384
#define CFG_CACHELINE_SIZE 32
 
#if (CONFIG_COMMANDS & CFG_CMD_KGDB)
# define CFG_CACHELINE_SHIFT 5 /*log base 2 of the above value*/
#endif
 
#define CFG_RCWH_PCIHOST 0x80000000 
 
#define ADD_HRCW_DEVICE (                \
HRCWH_BOOTSEQ_DISABLE |\
HRCWH_FROM_0X00000100 |\
HRCWH_ROM_LOC_NAND_LP_16BIT |\
HRCWH_RL_EXT_LEGACY |\
0)
 
#define ADD_HRCW_NET (         \
        HRCWH_TSEC1M_IN_SGMII |\
      HRCWH_TSEC2M_IN_SGMII |        \
      0)
 
#define CFG_HRCW_HIGH (         \
       ADD_HRCW_DEVICE |        \
       ADD_HRCW_NET |        \
       HRCWH_PCI_HOST |        \
       HRCWH_PCI1_ARBITER_ENABLE |\
       HRCWH_CORE_ENABLE |\
       HRCWH_SW_WATCHDOG_DISABLE |\
       HRCWH_BIG_ENDIAN |\
       HRCWH_LALE_NORMAL |\
       0)
 
/* 
 * 33MHz IN, 166MHz CSB, 333 DDR, 333 CORE 
 */
#define CFG_HRCW_LOW (\
      HRCWL_LCL_BUS_TO_SCB_CLK_1X1 |\
      HRCWL_INIT |\
      HRCWL_DDR_TO_SCB_CLK_2X1 |\
      HRCWL_CSB_TO_CLKIN_5X1 |\
      HRCWL_CORE_TO_CSB_2X1 |\
      0)
 
/* 
 * System IO Config 
 */
 
//#define CFG_SICRH       (0x0) /* 3.3v @ 40 ohms */
#define CFG_SICRH       (1<<(31-7)) /* use TSEC clock, 3.3v @ 40 ohms */
//#define CFG_SICRL (0x30000000)
#define CFG_SICRL (0x33FC0000) //// enable GPIO 28 29 30 31
 
 
#define CFG_HID0_INIT 0x000000000
#define CFG_HID0_FINAL HID0_ENABLE_MACHINE_CHECK
 
#define CFG_HID2 HID2_HBE
 
/* 
 * DDR @ 0x00000000 
 */
#define CFG_IBAT0L (CFG_SDRAM_BASE | BATL_PP_10   | BATL_MEMCOHERENCE)
#define CFG_IBAT0U (CFG_SDRAM_BASE | BATU_BL_256M | BATU_VS | BATU_VP)
 
/* 
 * PCI @ 0x80000000 
 */
#define CONFIG_PCI
 
/*
 * General PCI
 * Addresses are mapped 1-1.
 */
 
#ifdef CONFIG_PCI
 
# define CONFIG_PCI_PNP
 
# undef  CONFIG_PCI_SCAN_SHOW
 
# define CFG_PCI_SUBSYS_VENDORID 0x1057
 
# define CFG_PCI1_MEM_BASE0x80000000
# define CFG_PCI1_MEM_PHYSCFG_PCI1_MEM_BASE
# define CFG_PCI1_MEM_SIZE 0x10000000 /* 256M */
 
# define CFG_PCI1_MMIO_BASE0x90000000
# define CFG_PCI1_MMIO_PHYSCFG_PCI1_MMIO_BASE
# define CFG_PCI1_MMIO_SIZE 0x10000000 /* 256M */
 
#define CFG_PCI1_IO_BASE0x00000000
#define CFG_PCI1_IO_PHYS0xE2000000
#define CFG_PCI1_IO_SIZE 0x00100000 /* 1M */
 
# define CFG_IBAT1L (CFG_PCI1_MEM_BASE  | BATL_PP_10   | BATL_MEMCOHERENCE)
# define CFG_IBAT1U (CFG_PCI1_MEM_BASE  | BATU_BL_256M | BATU_VS | BATU_VP)
 
# define CFG_IBAT2L (CFG_PCI1_MMIO_BASE | BATL_PP_10   | BATL_CACHEINHIBIT | BATL_GUARDEDSTORAGE)
# define CFG_IBAT2U (CFG_PCI1_MMIO_BASE | BATU_BL_256M | BATU_VS | BATU_VP)
# if defined(CONFIG_SCRDB_8313) || defined(CONFIG_ORION_8313) || defined(CONFIG_SCIMC) || defined(CONFIG_FRISER_8313) || defined(CONFIG_PTPIN) || defined(CONFIG_FIBER) ||defined(CONFIG_LF7520) || defined(CONFIG_LF7550)|| defined(CONFIG_LF7511)
#  define CONFIG_NATSEMI
#  undef  NATSEMI_DEBUG
# endif
 
# ifndef CONFIG_PCI_PNP
#  define PCI_IDSEL_NUMBER 0x0c /* slot0->3(IDSEL)=12->15 */
#  define PCI_ENET0_IOADDR 0x80000000
#  define PCI_ENET0_MEMADDR 0x80000000
# endif
 
#else
 
# define CFG_IBAT1L (0)
# define CFG_IBAT1U (0)
# define CFG_IBAT2L (0)
# define CFG_IBAT2U (0)
 
#endif
 
/* 
 * PCI2 not supported on 8313 
 */
 
#if 1
 
#define CFG_IBAT3L (0xE8000000 | BATL_PP_10 | BATL_MEMCOHERENCE)
/*#define CFG_IBAT4L (0xD0000000 | BATL_PP_10 | BATL_CACHEINHIBIT | BATL_GUARDEDSTORAGE)*/
#define CFG_IBAT3U (0xE8000000 | BATU_BL_64M | BATU_VS | BATU_VP)
 
#define CFG_IBAT4L (0xD0000000 | BATL_PP_10 | BATL_MEMCOHERENCE)
/*#define CFG_IBAT4L (0xD0000000 | BATL_PP_10 | BATL_CACHEINHIBIT | BATL_GUARDEDSTORAGE)*/
#define CFG_IBAT4U (0xD0000000 | BATU_BL_256M | BATU_VS | BATU_VP)
#else
/*modify byll 20210401*/
#define CFG_IBAT3L (0)
#define CFG_IBAT3U (0)
#define CFG_IBAT4L (0)
#define CFG_IBAT4U (0)
#endif
 
 
 
/* 
 * IMMRBAR @ 0xE0000000, PCI IO @ 0xE2000000 & BCSR @ 0xE2400000 
 */
#define CFG_IBAT5L (CFG_IMMR  | BATL_PP_10 | BATL_CACHEINHIBIT | BATL_GUARDEDSTORAGE)
#define CFG_IBAT5U (CFG_IMMR | BATU_BL_256M | BATU_VS | BATU_VP)
 
 
 
/* 
 * SDRAM @ 0xF0000000, stack in DCACHE 0xFDF00000 & FLASH @ 0xFE000000 
MODIFY BY LL 20210331
*/
#define CFG_IBAT6L (0xF0000000 | BATL_PP_10   | BATL_MEMCOHERENCE)
#define CFG_IBAT6U (0xF0000000 | BATU_BL_256M | BATU_VS | BATU_VP)
 
#define CFG_IBAT7L (0)
#define CFG_IBAT7U (0)
 
#define CFG_DBAT0L CFG_IBAT0L
#define CFG_DBAT0U CFG_IBAT0U
#define CFG_DBAT1L CFG_IBAT1L
#define CFG_DBAT1U CFG_IBAT1U
#define CFG_DBAT2L CFG_IBAT2L
#define CFG_DBAT2U CFG_IBAT2U
#define CFG_DBAT3L CFG_IBAT3L
#define CFG_DBAT3U CFG_IBAT3U
#define CFG_DBAT4L CFG_IBAT4L
#define CFG_DBAT4U CFG_IBAT4U
#define CFG_DBAT5L CFG_IBAT5L
#define CFG_DBAT5U CFG_IBAT5U
#define CFG_DBAT6L CFG_IBAT6L
#define CFG_DBAT6U CFG_IBAT6U
#define CFG_DBAT7L CFG_IBAT7L
#define CFG_DBAT7U CFG_IBAT7U
 
/*
 * Internal Definitions
 *
 * Boot Flags
 */
#define BOOTFLAG_COLD 0x01 /* Normal Power-On: Boot from FLASH */
#define BOOTFLAG_WARM 0x02 /* Software reboot */
 
#define UBOOT_BAUDRATE 115200
 
 
#if (CONFIG_COMMANDS & CFG_CMD_KGDB)
# define CONFIG_KGDB_BAUDRATE UBOOT_BAUDRATE /* speed of kgdb serial port */
# define CONFIG_KGDB_SER_INDEX 2 /* which serial port to use */
#endif
/*
 * Environment Configuration
 */
#undef CONFIG_VERSION_VARIABLE
 
#define CONFIG_ENV_OVERWRITE
#define CONFIG_NET_MULTI
#define CONFIG_BOOTFILE uImage
#define CONFIG_SERVERIP 192.168.1.123  /*81.128*/
 
#undef  CONFIG_SHOW_BOOT_PROGRESS
 
#define CFG_LOAD_ADDR           100000
#define CONFIG_LOADADDR         CFG_LOAD_ADDR
 
#define  CONFIG_AUTOBOOT_KEYED
#define  CONFIG_AUTOBOOT_PROMPT "Boot in %d seconds\n"
#define  CONFIG_AUTOBOOT_DELAY_STR "."
 
#define CONFIG_BOOTDELAY 3 /* -1 disables auto-boot */
#define CONFIG_BAUDRATEUBOOT_BAUDRATE
 
/*
 * JFFS2 configuration + mtdparts
 */
 
#define CONFIG_JFFS2_NAND
#define CONFIG_JFFS2_DEV        "nand0"
#define CONFIG_JFFS2_CMDLINE
 
# if 1
/* should be the same for all of our 8313 designs */
#define MTDIDS_DEFAULT "nand0=s8313.nand"
#define MTDPARTS_DEFAULT        "mtdparts=mtdparts=s8313.nand:" \
                                "128k(stage0),"        \
                                "896k(boot),"          \
                                "1m(factory),"          \
                                "1m(control)"
 
/* may vary depending on amount of NAND or other considerations */
#define CONFIG_MTDPARTS         MTDPARTS_DEFAULT       \
                                ","                    \
                                "16m(os.1),"           \
"8m(uImage.1),"        \
                                "16m(os.2),"           \
"8m(uImage.2),"        \
                                "76m(appl.1),"         \
                                "76m(appl.2),"         \
                                "8m(config.1),"        \
                                "8m(config.2),"        \
                                "-(pst)"               \
                                "\0"
 
 
#else
#define MTDIDS_DEFAULT "nor0=s8313.flash,nand0=s8313.nand"
#define MTDPARTS_DEFAULT        "mtdparts=mtdparts=s8313.flash:" \
"2m(uboot),"\
"s8313.nand:128k(stage0),"   \
                                "896k(boot),"          \
                                "1m(factory),"          \
                                "1m(control)" \
"16m(os.1),"          \
"8m(uImage.1),"        \
                                "16m(os.2),"            \
"8m(uImage.2),"        \
                                "76m(appl.1),"          \
                                "76m(appl.2),"          \
                                "8m(config.1),"        \
                                "8m(config.2),"        \
                                "30m(pst)" \
/* may vary depending on amount of NAND or other considerations */
#define CONFIG_MTDPARTS         MTDPARTS_DEFAULT        \
                                "\0"
#endif 
#define NAND_CACHE_PAGES 4
 
/* 
 * Manufacturing/devlopment scripts to write to NAND flash 
 */
 
#define CONFIG_HAS_ETH1
 
 
#  define CONFIG_TARGET            "LF7511"
#  define CONFIG_ETHPRIME          "TSEC1"
#  define CONFIG_HOSTNAME        "LF7511"
#  define CONFIG_IPADDR            192.168.1.113    /*81.113*/
#  define CONFIG_ETHADDR          78:CA:83:BF:05:6A
#  define CONFIG_ETH1ADDR          78:CA:83:BF:05:6B
 
 
 
 
 
 
#define CONFIG_NEW_STAGE0 "wstage0="     \
  "tftp $loadaddr ${target}/u-boot-spl.bin && "     \
  "nand erase stage0 && "     \
  "nand write.jffs2 $fileaddr stage0 $filesize"     \
  "\0"
 
#define CONFIG_NEW_BOOT "wboot="     \
  "tftp $loadaddr ${target}/u-boot.bin && "     \
  "nand erase boot && "     \
  "nand write.jffs2 $fileaddr boot $filesize"     \
  "\0"
 
/* 
 * force the size to 0x800000 since the write has to be 
 * on a and 0x800000 is larger than we can currently
 * build to...
 */
 
#define CONFIG_NEW_UIMAGE "wuimage="                    \
  "tftp $loadaddr ${target}/uImage ;  "                 \
  "if test $? -gt 0 ; then "                            \
    "test 1=2 ; "                                       \
  "else "                                               \
    "nand erase uImage.1 ; " \
    "nand erase uImage.2 ; " \
    "nand write $fileaddr uImage.1 800000 ; "           \
    "nand write $fileaddr uImage.2 800000 ; "           \
  "fi"                                                  \
  "\0"
 
#define CONFIG_NEW_OS "wos="     \
  "tftp $loadaddr ${target}/os.jffs2 && "                   \
  "nand erase os.1 && "     \
  "nand erase os.2 && "     \
  "nand write.jffs2 $fileaddr os.1 $filesize && "     \
  "nand write.jffs2 $fileaddr os.2 $filesize && "     \
  "run wuimage "                                            \
  "\0"
 
#define CONFIG_NEW_CONTROL "wcontrol="     \
  "tftp $loadaddr ${target}/control.jffs2 && "     \
  "nand erase control && "     \
  "nand write.jffs2 $fileaddr control $filesize"     \
  "\0"
 
#define CONFIG_NEW_FACTORY "wfactory="     \
  "tftp $loadaddr ${target}/factory.jffs2 && "     \
  "nand erase factory && "     \
  "nand write.jffs2 $fileaddr factory $filesize"     \
  "\0"
 
/* 
 * do not write uImage here --- wait until everything
 * else is writtent so if it fails there will be enough
 * left over to fix the problem in linux
 */
 
#define CONFIG_NEW_OSS "woss="     \
  "run wstage0 && "     \
  "run wboot && "     \
  "run wos && "     \
  "run wcontrol"     \
  "\0"
 
#define CONFIG_NEW_APPL "wappl="     \
  "tftp $loadaddr ${target}/appl.jffs2 && "     \
  "nand erase appl.1 && "     \
  "nand write.jffs2 $fileaddr appl.1 $filesize && "     \
  "nand erase appl.2 && "     \
  "nand write.jffs2 $fileaddr appl.2 $filesize"     \
  "\0"
 
#define CONFIG_NEW_CONFIG "wconfig="         \
  "tftp $loadaddr ${target}/config.jffs2 && "         \
  "nand erase config.1 && "         \
  "nand write.jffs2 $fileaddr config.1 $filesize && " \
  "nand erase config.2 && "         \
  "nand write.jffs2 $fileaddr config.2 $filesize"       \
  "\0"
 
#define CONFIG_NEW_PST "wpst="     \
  "tftp $loadaddr ${target}/pst.jffs2 && "     \
  "nand erase pst && "     \
  "nand write.jffs2 $fileaddr pst $filesize"     \
  "\0"
 
#define CONFIG_NEW_MOST "wmost="     \
  "run woss && "     \
  "run wappl  && "     \
  "run wconfig && "     \
  "run wpst "     \
  "\0"
 
#define CONFIG_NEW_ALL "wall="                              \
  "run wmost && "     \
  "run wfactory ; "     \
  "if test $? -gt 0 ; then "     \
     "echo ERROR: UNABLE TO COMPLETE SOFTWARE LOAD ; "      \
  "else "     \
      "echo INFO: SOFTWARE LOAD COMPLETE ; "     \
  "fi"     \
  "\0"
 
/* 
 * Manufacturing/devlopment scripts to boot partitions 
 */
 
#define CONFIG_BA_R "bar=" \
  "symwdt ; " \
  "setenv bootargs " \
  "root=/dev/ram rw " \
  "rdinit=$start " \
  "console=ttyS0,$baudrate " \
  "${mtdparts} " \
  "next=$next " \
  "bprog=$bprog " \
  "last=$last " \
  "target=$target " \
  "wdt=$wdt " \
  "bver=$bver" \
  "\0"
 
#define CONFIG_BT_T   "boot.t=" \
  "chpart control ; " \
  "symscrl next.scr ; " \
  "symscrl last.scr ; " \
  "symlft ; " \
  "tftp $daddr ${target}/dtb && " \
  "tftp $kaddr ${target}/$bootfile && " \
  "run bar ; " \
  "bootm $kaddr - $daddr" \
  "\0"
 
#if defined(CONFIG_FRISER_8313)
 
/* not load fpga */
#define CONFIG_BT_NX   "boot.nx=" \
  "chpart os.${next} ; " \
  "fsload $daddr dtb ; " \
  "if test $? -gt 0 ; then " \
     "set bprog boot-dtb ; " \
     "test 1=2 ; "       \
  "else " \
     "run get.uImage && "         \
     "run bar && " \
     "bootm $kaddr - $daddr ; " \
     "if test $? -gt 0 ; then " \
        "set bprog boot-fallback && " \
        "run get.uImage.j && "                \
        "run bar && " \
        "bootm $kaddr - $daddr ; " \
     "fi ; " \
  "fi ; " \
  "\0"
 
#elif 1
 
/* fail of fpga load fails boot */
#define CONFIG_BT_NX   "boot.nx=" \
  "chpart os.${next} && " \
  "symlfl ; " \
  "if test $? -gt 0 ; then " \
    "set bprog boot-fpga ; " \
    "test 1=2 ; "         \
  "else " \
    "fsload $daddr dtb ; " \
    "if test $? -gt 0 ; then " \
      "set bprog boot-dtb ; " \
      "test 1=2 ; "       \
    "else " \
       "run get.uImage && "         \
       "run bar && " \
       "bootm $kaddr - $daddr ; " \
       "if test $? -gt 0 ; then " \
          "set bprog boot-fallback && " \
          "run get.uImage.j && "                \
          "run bar && " \
          "bootm $kaddr - $daddr ; " \
       "fi ; " \
    "fi ; " \
  "fi ; " \
  "\0"
 
#else
 
/* fail of fpga load - boot conintues */
#define CONFIG_BT_NX   "boot.nx=" \
  "chpart os.${next} ; " \
  "symlfl ; " \
  "if test $? -gt 0 ; then " \
    "set bprog boot-fpga ; " \
  "fi ; " \
  "fsload $daddr dtb ; " \
  "if test $? -gt 0 ; then " \
    "set bprog boot-dtb ; " \
  "fi ; "         \
  "run get.uImage && "         \
  "run bar && " \
  "bootm $kaddr - $daddr ; " \
  "if test $? -gt 0 ; then " \
    "set bprog boot-fallback ; " \
    "run get.uImage.j && "         \
    "run bar && " \
    "bootm $kaddr - $daddr ; " \
  "fi "                                         \
  "\0"
 
#endif
 
#define CONFIG_BT_1  "boot.1=" \
  "set next 1 ; "    \
  "set bprog boot-ok-1 ; " \
  "run boot.nx ; " \
  "if test $? -gt 0 ; then " \
    "set next 2 ; " \
    "set bprog boot-swap-2 ; "                 \
    "run boot.nx ; " \
  "fi" \
  "\0"
 
#define CONFIG_BT_2  "boot.2="                 \
  "set next 2 ; "                                \
  "set bprog boot-ok-2 ; "                       \
  "run boot.nx ; "                               \
  "if test $? -gt 0 ; then "                     \
    "set next 1 ; "                              \
    "set bprog boot-swap-1 ; "                   \
    "run boot.nx ; "                             \
  "fi"                                           \
  "\0"
 
#define CONFIG_BT_N  "boot.n="     \
  "chpart control ; " \
  "symscrl next.scr ; " \
  "symscrl last.scr ; " \
  "if test ${next} -eq 1 ; then " \
    "run boot.1 ; " \
  "else " \
    "run boot.2 ; " \
  "fi ; " \
  "symblnk " \
  "\0"
 
#define CONFIG_GET_UIMAGE "get.uImage=" \
  "echo BOOT FROM UIMAGE ; symuimage $kaddr uImage.${next} 0" \
  "\0"
 
#define CONFIG_GET_UIMAGE_J "get.uImage.j=" \
  "echo BOOT FROM JFFS2 ; fsload $kaddr $bootfile" \
  "\0"
 
#define XMK_STR(x) #x
#define MK_STR(x) XMK_STR(x)
 
/* "bver=\"" CONFIG_TARGET " (" __DATE__ " "__TIME__ ")\"\0"  */
 
#if defined(CONFIG_SCRDB_8313)
#define SYMM_BUILD_NAME CONFIG_SCRDB_8313_BLD
#elif defined(CONFIG_FRISER_8313)
#define SYMM_BUILD_NAME CONFIG_FRISER_8313_BLD
#elif defined(CONFIG_ORION_8313)
#define SYMM_BUILD_NAME CONFIG_ORION_8313_BLD
#elif defined(CONFIG_SM1000)
#define SYMM_BUILD_NAME CONFIG_SM1000_BLD
#elif defined(CONFIG_SM2000_MC)
#define SYMM_BUILD_NAME CONFIG_SM2000_MC_BLD
#elif defined(CONFIG_SM2000_CC)
#define SYMM_BUILD_NAME CONFIG_SM2000_CC_BLD
#elif defined(CONFIG_LF7300)
#define SYMM_BUILD_NAME CONFIG_LF7300_BLD
#elif defined(CONFIG_LF7520)
#define SYMM_BUILD_NAME CONFIG_LF7520_BLD
#elif defined(CONFIG_LF7560)
#define SYMM_BUILD_NAME CONFIG_LF7560_BLD
#elif defined(CONFIG_LF7550)
#define SYMM_BUILD_NAME CONFIG_LF7550_BLD
#elif defined(CONFIG_LF7511)
#define SYMM_BUILD_NAME CONFIG_LF7511_BLD
#else
#define SYMM_BUILD_NAME CONFIG_SM2000_BLD
#endif
 
#define CONFIG_EXTRA_ENV_SETTINGS \
  "target=" CONFIG_TARGET "\0"         \
  "ethprime=" CONFIG_ETHPRIME "\0" \
  "kaddr=F000000\0" \
  "daddr=FE00000\0" \
  "start=linuxrc\0"         \
  "next=1\0"         \
  "bprog=undefined\0" \
  "fpgaName=fpga\0" \
  "bver=\"" SYMM_BUILD_NAME "\"\0" \
  CONFIG_MTDPARTS \
  CONFIG_GET_UIMAGE \
  CONFIG_GET_UIMAGE_J \
  CONFIG_NEW_STAGE0 \
  CONFIG_NEW_BOOT \
  CONFIG_NEW_OS \
  CONFIG_NEW_UIMAGE \
  CONFIG_NEW_FACTORY \
  CONFIG_NEW_CONTROL \
  CONFIG_NEW_OSS \
  CONFIG_NEW_APPL \
  CONFIG_NEW_CONFIG \
  CONFIG_NEW_PST \
  CONFIG_NEW_MOST \
  CONFIG_NEW_ALL \
  CONFIG_BA_R \
  CONFIG_BT_T                    \
  CONFIG_BT_NX                  \
  CONFIG_BT_NX \
  CONFIG_BT_1 \
  CONFIG_BT_2 \
  CONFIG_BT_N \
  "\0"
 
#define CONFIG_BOOTCOMMAND "run boot.n"
 
#endif /* __CONFIG_H */

 

 

0 件の賞賛
返信
4,431件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please specify TEXT_BASE as NOR FLASH start address 0xe8000000.

4,426件の閲覧回数
leilei987
Contributor II

 hi

yiping

I have tried to change my advice? ,But it didn't work

my private script:

ARCH = ppc
CPU = mpc83xx
BOARD = s8313
CONFIG_NAND_U_BOOT = y
CONFIG_NAND_LP = y

s8313? is? my private board name

it's base on mpc8313erdb config

I make sure I don't want the two bold lines of macro definition above

but modify to "n" the uboot.img size??It went from 325K to 275K,And tftp? not available

 

tftp
**bleep**: 0FFC1FD8 XER: 20000000 LR: 0FFC1258 REGS: 0ff10b58 TRAP: 0700 DAR: 0000B032
MSR: 0008b032 EE: 1 PR: 0 FP: 1 ME: 1 IR/DR: 11

GPR00: 0FFC1FD8 0FF10C48 00000080 00007949 0FF32CC8 00000001 00000000 00000000
GPR08: 00000004 00000000 0FFFD260 00000000 28022022 AB87FAF7 0FFF8000 0FFEEA5C
GPR16: 0FFF333C 00000000 00000000 00000000 00000000 00000000 00000000 0FF32CC8
GPR24: 0FF32C88 FFFFFFFF E0024000 0FFF89E0 0FF32CC8 0FF10F58 0FFF8790 0FFF40D8
Call backtrace:
0FFC1240 0FFC24D4 0FFBB76C 0FFBA094 0FFD0914 0FFD84D4 0FFD7B44
0FFD7CF4 0FFC8428 0FFB877C 0FFB46AC
Program Check Exception
resetting the board, address: 0ff00120

 

Reset Configuration Word High Register (RCWHR? ?BMS??Set 1 or 0
thanks

0 件の賞賛
返信
4,425件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please compile u-boot with configs/MPC8313ERDB_33_defconfig or MPC8313ERDB_66_defconfig.

Please modify your u-boot configuration based on include/configs/MPC8313ERDB.h.

0 件の賞賛
返信
4,394件の閲覧回数
leilei987
Contributor II

hi 

yiping

so good

This problem has been resolved 。

tank you very much!

best regards!

0 件の賞賛
返信
4,419件の閲覧回数
leilei987
Contributor II

oh  i can‘t  stand it any more

because  my uboot version is 1.1.6

there is no configs/MPC8313ERDB_33_defconfig or MPC8313ERDB_66_defconfig  file 

I took over the project in mid-stream,None of my colleagues knew much about it

in 1.1.6 version  my private .h  is based on include/configs/MPC8313ERDB.h

and i try download uboor code in qoriq sdk v1.9 

but Machine type not have 8313erdb!

I'm at the end of my tether

 

 

0 件の賞賛
返信