mc1322x reset modes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc1322x reset modes

1,358 次查看
SteveJ
Contributor I
Hi,

I'm trying to figure out if it's possible to detect the reason for aprocessor reset on the mc1322x. Specifically I'd like to detect if areset was due to a POR, SW_RST or watchdog fail.Any ideas?

Thanks, Steve.
标记 (1)
0 项奖励
回复
1 回复

1,237 次查看
TomE
Specialist II

The ColdFire chips have a Reset Reason Register. The Power chips (MPC5604 anyway) has a "Functional Event Status Register". Kinetis have "System Reset Status" registers. If the ARM Core doesn't have this internally, this chip doesn't seem to have this available.

 

> POR, SW_RST or watchdog fail.

 

The code that performs the SW_RST could leave some "magic values" in SRAM somewhere, as long as there's some SRAM that survives a reset.

 

I've always tried to have a very high priority software watchdog running slightly ahead of the hardware watchdog. So if the software one triggers you know the hardware one is about to, and the software one can print where the code is stuck or record the stack frame somewhere. You could do the same (have the software one leave some different "magic" in SRAM).

 

Tom

 

0 项奖励
回复