Hello Habib,
Thank you for the clarification.
However, I must admit that I am a bit frustrated with the way this question has been handled. In my initial message, I clearly described the tests I had already performed, including reading the GPIO_PSR registers and enabling SION. Your first reply simply suggested checking GPIO_PSR and reviewing the application note, which was information I had already explicitly mentioned.
Because of this, the response did not really address my actual question and led me to spend additional time re-explaining the same points.
What I was trying to understand from the beginning was whether the GPIO input path remains connected to the pad when the pin is muxed to a peripheral function (ALT6) on the i.MX RT1170. Your latest message finally clarifies that this is not supported with the UART module, which is the information I was looking for.
For future exchanges, I would appreciate if the initial question and the described tests could be reviewed more carefully, as this would help avoid unnecessary back-and-forth and save time on both sides.
Best regards.