load

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

load

1,025件の閲覧回数
qasim_ahtesham
Contributor I

Hi everyone,
I am looking to design an energy management system using microcontrollers. Essentially, I have to control 10 GPOs (9 two gang, and 1 four gang GPO) per house, and there are 20 houses (this means total 200 GPOs).
I need to measure the power flowing through them, as well as their state (on/off), and report this to the MASTER/Central MCU, which will not just be getting data from the 200 GPOs, but also from the Victron Server (via Modbus preferably). Based on the data received, I want to control each GPO (control whether it stays on, or should be turned off). The following diagrams can explain this better:

LA-ems-1.PNG

         Fig. 1

LA-ems-20.PNG

Fig. 2

LA_EMS.PNG

Fig.3

So, I am looking for a MCU which can communicate via Modbus, as well as via internet wirelessly, and via wire. Are there any similar designs available? More importantly, which MCUs will be the best choice for this project?


Thanks

タグ(1)
0 件の賞賛
返信
0 返答(返信)