linux login not available in debug terminal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux login not available in debug terminal

922件の閲覧回数
donjacobvellathottam
Contributor III

Hi,

I've built a linux image for imx8 board using yocto.

the linux works without any issues in the hardware. But I am not able to login to the system with a debug terminal from my linux pc using gtk terminal.

all other debug information up to boot and from shutdown to poweroff are coming in the gtk terminal, but the login prompt is not shown.

any suggestions as to why this is happening or how can i solve this ?

TIA

0 件の賞賛
返信
2 返答(返信)

903件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Connect your mx8 to the terminal and see if this works since we running console by default.

Regards

0 件の賞賛
返信

888件の閲覧回数
donjacobvellathottam
Contributor III

thanks for the reply,

i've booted the imx8 with the os and connected it to the gtk terminal.

i get debug updates upto the login but not the login option.

then it shows the updates while being powered down

 

0 件の賞賛
返信