kernel panic with booting eMMC on imx8navq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel panic with booting eMMC on imx8navq

2,330 Views
mmt45
Contributor I

Hello, I was following this guide to setup cognipilot on NavQPlus (imx8navq) https://airy.cognipilot.org/cranium/compute/navqplus/setup/#log-in-for-the-first-time ). After flashing the ubuntu image, I change the switches of Navq into eMMC mode (switch 1 off, switch 2 on), and when I screen into the UART connection from the terminal, I get a kernel panic error. It shows in the lines above that is related to ext4-fs. How can i solve the problem?

0 Kudos
Reply
2 Replies

2,281 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @mmt45 

I hope you are doing well.

 

Could you please contact to your sales person?

We cannot provide support for this board.

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply

2,313 Views
mmt45
Contributor I

Screenshot from 2024-08-19 15-10-21.pngScreenshot from 2024-08-19 15-10-21.png

this is another screenshot from the terminal

0 Kudos
Reply