imx93 FRDM mac address randomisation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 FRDM mac address randomisation

1,346 Views
sakshi123
Contributor I

I am working with an i.MX93 FRDM board running the base image provided by NXP (link: "https://github.com/nxp-imx/meta-imx"). The issue I’m facing is that the MAC address changes every time the board is powered on. Is there an image available in which the MAC address remains fixed across reboots and does not change?

Currently, because the MAC address keeps changing on each reboot, the pool of allowed MAC addresses gets exhausted, preventing other devices from connecting to the network.

We are specifically looking for a solution at the image level, not through any additional service or workaround

0 Kudos
Reply
3 Replies

1,323 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @sakshi123 

 

I would suggest you configure a MAC address using ifconfig.  you can use the following command:

ifconfig <interface> hw ether <MAC-address>

For example:  ifconfig eth0 hw ether 00:11:22:33:44:55

 

Regards

Daniel

0 Kudos
Reply

1,281 Views
sakshi123
Contributor I

I have a follow-up question regarding the MAC address for the i.MX93 FRDM board.

From the i.MX93 FRDM datasheet (screenshot attached below), it is mentioned that:

sakshi123_2-1759483198532.png



Question is : Is there any physical setup on the i.MX93 board to configure or set a static MAC address for every bootup, or is the MAC address always fused and fixed inside the i.MX93 processor?

 

0 Kudos
Reply

1,214 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi,

 

Please refer to below link to write MAC address.

Solved: i.MX91 fusemap spreadsheet needed to write MAC addresses into OTP - NXP Community

 

Regards

Daniel

0 Kudos
Reply