imx-21 and emma_binary

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-21 and emma_binary

2,346 次查看
MarcelWISE
Contributor I
Hi
I'm developing a project with imx-21 arm processor in company where I work (Wise Indústria de Telecomunicações from Brazil). I want implemented video decoder in board with imx21, I use hantro decoder, emma player (emma-binary-mx21-2.0) and linux kernel 2.4.20.

I need compile the package emma-binary-mx21-2.0, especially emma-play, because I need to increase the variable rtp.size in emma_play.c. But to recompile the source code, I need file config.mak, included in emma_play makefile, because the package emma-binary-mx21-2.0, don't contains this file.

How do I do to get the file config.mak of emma-binary-mx21-2.0???

I use ltib (BSP version TO3.2), the emma-binary is package from Ltib. I already try recompile using Ltib, but I don't get sucess, because Ltib don't make the new executables.

How do I do to recompile emma-binary???

Thanks


Message Edited by MarcelWISE on 2008-05-15 06:14 PM
0 项奖励
回复
1 回复

1,620 次查看
Mondial
Contributor I
Hi Marcel,

there is a fix from Freescale for the makefile. They promised to include the fix in the next release for the BSP, but I'll assume there wont be any new release for the i.MX21 anymore (the same will apply to the WinCE BSP :smileysad:

Contact the Freescale support for "Makefile_mx21_emma_demo_fix" .

Also, dont forget to take a look at the Hantro licensing.

Regards,
Christian
0 项奖励
回复