if bfu725 can be used in Ka band

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

if bfu725 can be used in Ka band

711件の閲覧回数
hanjingwen1988
Contributor I

IN BFU725 data sheet , the applications includes Ka-Band DRO, but i notice that the S-PARA is only gived to 26GHz, but Ka band is about 26.5-40GHz, so i dont know whether this transistor can be used in Ka-Band oscillator design.

0 件の賞賛
返信
2 返答(返信)

632件の閲覧回数
LPP
NXP Employee
NXP Employee

BFU725F has Ft = 55GHz.
It can be used for DRO oscillator up to ~30GHz (checked) and ~35GHz (with doubt).


Have a great day,
Pavel
NXP TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

632件の閲覧回数
hanjingwen1988
Contributor I

Thanks for your reply.

And I still don’t understand that if the S-para only gives to 26G, how can I confirm the correctness of the model. In other words, I’m worried about the simulation results is different from the Actual circuit.

In your experience, is that a problem that I should worried?

Looking forward to your reply.

Thanks again!!

Jingwen Han

2019.09.06

发送自 Windows 10 版邮件<https://go.microsoft.com/fwlink/?LinkId=550986>应用

0 件の賞賛
返信