iMX6 SABRE AI Board / Android Automotive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 SABRE AI Board / Android Automotive

1,125 Views
developers1
Contributor I

Hello,

We are currently investigating AndroidAutomotive/AGL(AutomotiveGradeLinux).
The purpose is to perform the authorization process using Ipod Auth Module(AUTHIC 2.0C or 3.0C) while AndroidAutomotive or AGL(AutomotiveGradeLinux) is active.

Q1:
We have iMX6 SABRE AI Board.
We found the source tree for Android8.0 (imx-o8.0.0_1.0.0_ga.tar.gz).
However we have not found the source tree for AndroidAutomotive yet.
https://source.android.com/devices/automotive

Is AndroidAutomotive not officially supported ?


Q2:
Also we searched for the BSP environment for AGL(AutomotiveGradeLinux), but we could not find it.
Is AGL not supported ?

0 Kudos
Reply
3 Replies

960 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The AGL is supported, you can see the meta-nxp-agl.git - NXP AGL Yocto Project Demo Layer 

Compile command is as following:

DISTRO=nxp-imx-agl-wayland MACHINE=imx6qsabresd source nxp-setup-agl.sh -b bld-agl
bitbake agl-demo-platform

You can refer to. I have not tried it. Hope this can do help for you.

Have a ncie day

Rita

0 Kudos
Reply

960 Views
manizillion
Contributor IV

Hi Rita,

The repo sync is not succeeding at all in the link you had sent for AGL build, kindly share the  link with correct steps, or is there a fix for this ? too many steps for imx is floating around, NXP can show us correct pointers to refer the steps. We are using nxp extensively.

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.0.0-agl-demo.xml

Fetching projects:  86% (13/15)
Fetching project meta-fsl-bsp-release
remote: Counting objects: 102054, done.        
remote: Compressing objects: 100% (31874/31874), done.       
error: Cannot fetch DemoApps/CES2016 from https://gerrit.automotivelinux.org/gerrit/AGL/DemoApps/CES2016
remote: Total 102054 (delta 62576), reused 97678 (delta 58476) 

Fetching projects:  93% (14/15)

error: Exited sync due to fetch errors

Thanks and Regards

Mani

0 Kudos
Reply

960 Views
developers1
Contributor I

Thank you for your prompt reply.
I'll give it a try.

0 Kudos
Reply