imx6q sabresd board could not running for android P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q sabresd board could not running for android P

2,271 Views
zhangmike
Contributor II

Hi:

My board is imx6q sabresd.

Enviroment: android9.0

My kernel is started, but it hangs when it boots up to android .  I don't know why

log is here:

Connecting to /dev/ttyUSB1, speed 115200
 Escape character: Ctrl-\ (ASCII 28, FS): enabled
Type the escape character followed by C to get back,
or followed by ? to see other options.
----------------------------------------------------
∙
U-Boot 2018.03 (Jul 25 2019 - 14:30:30 +0800)
CPU:   Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 53C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  2 GiB
MMC:   ∙∙
U-Boot 2018.03 (Jul 25 2019 - 14:30:30 +0800)
CPU:   Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 57C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  2 GiB
MMC:   ∙
U-Boot 2018.03 (Jul 25 2019 - 14:29:58 +0800)
CPU:   Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 55C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  2 GiB
MMC:   FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
flash target is MMC:0
Net:   No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  3 2 1 0
RNG already instantiated 0x40000003
Error: blob decap job failed 0x2000081a
Error during blob decap operation: 0x2000081a
In boota get fastboot lock status error. Set lock status
RNG already instantiated 0x40000003
RNG already instantiated 0x40000003
 verify OK, boot 'boot'
kernel   @ 14008000 (9729104)
ramdisk  @ 15000000 (1834834)
fdt      @ 14f00000 (54566)
## Booting Android Image at 0x14007800 ...
Kernel load addr 0x14008000 size 9502 KiB
## Flattened Device Tree blob at 14f00000
   Booting using the fdt blob at 0x14f00000
   XIP Kernel Image ... OK
   Using Device Tree in place at 14f00000, end 14f10525
switch to ldo_bypass mode!
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 4.14.98 (mikezhang@sileadinc) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #8 SMP PREEMPT Tue Jul 9 19:31:01 CST 2019
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
Memory policy: Data cache writealloc
cma: Reserved 320 MiB at 0x2a000000
random: get_random_bytes called from start_kernel+0xac/0x450 with crng_init=0
percpu: Embedded 18 pages/cpu @f64e6000 s41292 r8192 d24244 u73728
Built 1 zonelists, mobility grouping on.  Total pages: 522290
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,fbpix=RGB32,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=128M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=320M galcore.contiguousSize=33554432 loop.max_part=7 buildvariant=eng androidboot.serialno=201779d4df645324 androidboot.btmacaddr=20:17:79:d4:df:64 androidboot.soc_type=imx6q androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:5443,KL:0,KD:0,AVB:924,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.verifiedbootstate=green androidboot.slot_suffix= androidboot.vbmeta.device=PARTUUID=217671dd-2535-4cbe-95a8-25246f6ee45d androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked androidboot.vbmeta.hash_alg=sha256 androidboot.vbmeta.size=2944 androidboot.vbmeta.digest=0fa45b0d656f2600738c9c74cd83cbf8900b1b2911be5f886c028b446e244c9a androidboot.veritymode=enforcing androidboot.dtbo_idx=0 androidboot.keystore=soft
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1725244K/2097152K available (13312K kernel code, 1031K rwdata, 3880K rodata, 1024K init, 502K bss, 44228K reserved, 327680K cma-reserved, 1187840K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xf8000000 - 0xff800000   ( 120 MB)
    lowmem  : 0xc0000000 - 0xf7800000   ( 888 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc0e00000   (14304 kB)
      .init : 0xc1300000 - 0xc1400000   (1024 kB)
      .data : 0xc1400000 - 0xc1501f48   (1032 kB)
       .bss : 0xc1503000 - 0xc1580800   ( 502 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
ftrace: allocating 40592 entries in 120 pages
Preemptible hierarchical RCU implementation.
 Tasks RCU enabled.
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux:  Initializing.
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU2: Spectre v2: using BPIALL workaround
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
CPU3: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
vdd1p1: supplied by regulator-dummy
vdd3p0: supplied by regulator-dummy
vdd2p5: supplied by regulator-dummy
vddarm: supplied by regulator-dummy
vddarm: failed to get the current voltage(-22)
anatop_regulator 20c8000.anatop:regulator-vddcore: failed to register vddarm
anatop_regulator: probe of 20c8000.anatop:regulator-vddcore failed with error -22
vddpu: supplied by regulator-dummy
vddsoc: supplied by regulator-dummy
vddsoc: failed to get the current voltage(-22)
anatop_regulator 20c8000.anatop:regulator-vddsoc: failed to register vddsoc
anatop_regulator: probe of 20c8000.anatop:regulator-vddsoc failed with error -22
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins or pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/gpio_leds/gpioledsgrp
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx rpmsg driver is registered.
pstore: using zlib compression
console [pstore-1] enabled
pstore: Registered ramoops as persistent store backend
ramoops: attached 0x100000@0x3ff00000, ecc: 0/0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usb_phy_generic 2000000.aips-bus:usbphy_nop1: 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
usb_phy_generic 2000000.aips-bus:usbphy_nop2: 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1792K
hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.690:1): state=initialized audit_enabled=0 res=1
workingset: timestamp_bits=14 max_order=19 bucket_order=5
Registering sdcardfs 0.1
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
pwm-backlight backlight: backlight supply power not found, using dummy regulator
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
############################begin: set lcd power##########################
xxxxxxxxxldb_probe, line=710, lcd_tcon_en=39!
xxxxxxxxxldb_probe, line=724, mblpw=86!
ldb 2000000.aips-bus:ldb: xxxxxrequest mblpw gpio failed:-16
xxxxxxxxxldb_probe, line=738, dmipls=126!
############################end: set lcd power##########################
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2000000.aips-bus:ldb; cannot claim for lcd@0
imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd@0) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 (MX6Q_PAD_DISP0_DAT9) from group ipu1grp  on device 20e0000.iomuxc
mxc_lcdif lcd@0: Error applying setting, reverse things back
mxc_lcdif: probe of lcd@0 failed with error -22
mxc_sdc_fb fb@0: registered mxc display driver ldb
Console: switching to colour frame buffer device 100x30
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: Falling back to user helper
mxs-dma 110000.dma-apbh: initialized
imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
i2c i2c-1: SCL is stuck low, exit recovery
pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
pfuze100-regulator: probe of 1-0008 failed with error -11
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 73, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Added device: zram0
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
CAN device driver interface
fec 2188000.ethernet: 2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 1a:22:ba:7d:c0:3a
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 2184800.usbmisc: 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.14.98 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
<<-GTP-INFO->> GTP driver installing...
<<-GTP-INFO->> GTP Driver Version: V2.2<2014/01/14>
<<-GTP-INFO->> GTP I2C Address: 0x5d
<<-GTP-INFO->> Guitar reset
<<-GTP-INFO->> IC Version: 911_1060
<<-GTP-INFO->> X_MAX: 0, Y_MAX: 0, TRIGGER: 0x00
<<-GTP-INFO->> create proc entry gt9xx_config success
input: goodix-ts as /devices/virtual/input/input0
gpio gpiochip4: (20ac000.gpio): gpiochip_lock_as_irq: tried to flag a GPIO set as output for IRQ
gpio-mxc 20ac000.gpio: unable to lock HW IRQ 6 for IRQ
genirq: Failed to request resources for gd111x (irq 216) on irqchip gpio-mxc
<<-GTP-ERROR->> Request IRQ failed!ERRNO:-22.
<<-GTP-INFO->> GTP works in polling mode.
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
ov564x 0-003c: cannot get io voltage
ov564x 0-003c: cannot get core voltage
ov564x 0-003c: cannot get analog voltage
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
ov5642_power_on: cannot get io voltage error
ov5642_power_on: cannot get core voltage error
ov5642_power_on: cannot get analog voltage error
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
ov5640_power_on: cannot get io voltage error
ov5640_power_on: cannot get core voltage error
ov5640_power_on: cannot get analog voltage error
i2c i2c-1: SCL is stuck low, exit recovery
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
__power_supply_register: Expected proper parent device for 'battery'
(NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
__power_supply_register: Expected proper parent device for 'usb'
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffff5 is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
mma8x5x 0-001c: read chip ID 0xfffffffa is not equal to 0x1a,0x2a,0x3a,0x4a,0x5a!
mma8x5x: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: dm-devel@redhat.com
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
bt power gpio is:2
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_bt_rfkill driver success loaded
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
OF: /soc/aips-bus@02000000/vpu_fsl@02040000: could not get #power-domain-cells for /soc/aips-bus@02000000/gpc@020dc000
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_hdmi_cec soc:hdmi_cec@00120000: HDMI CEC initialized
Galcore version 6.2.4.190076
mmc0: new DDR MMC card at address 0001
mmcblk0: mmc0:0001 MMC08G 7.25 GiB
mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
mmcblk0rpmb: mmc0:0001 MMC08G partition 3 128 KiB
Alternate GPT is invalid, using primary GPT.
 mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13
[drm] Initialized vivante 1.0.0 20170808 for 130000.gpu on minor 1
caam 2100000.caam: ERA source: CAAMVID.
caam 2100000.caam: AXI pipeline throttling enabled.
caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0, dpaa2 = no
random: fast init done
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] b3 63 7b 30 85 ef aa 1f
platform caam_sm: [0008] f8 0a d4 58 d9 98 2a d3
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] a3 b0 d4 cd 25 7c 93 85
platform caam_sm: [0008] 11 e3 6d 53 b3 61 d8 fd
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] d0 95 82 89 34 00 89 d2
platform caam_sm: [0008] 45 f9 f6 13 80 46 30 e8
platform caam_sm: [0016] 5f 42 98 1f 74 6f 53 e8
platform caam_sm: [0024] a3 21 13 ae 79 36 c4 b5
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 64 10 86 14 9a ac c4 99
platform caam_sm: [0008] 0d 9e c1 1d eb dd d1 5f
platform caam_sm: [0016] 33 0f f0 e2 93 2a aa 13
platform caam_sm: [0024] d8 21 94 51 90 49 3f 76
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 41 b7 d3 ee f1 55 ee a4
platform caam_sm: [0008] cc 7a e5 3c 5c df 76 28
platform caam_sm: [0016] 1c 46 3b a4 c7 8a 25 d5
platform caam_sm: [0024] a1 f5 7b d8 ce b5 cb 44
platform caam_sm: [0032] 1b 4f 46 e3 95 b8 ab a4
platform caam_sm: [0040] c8 53 7f 25 27 89 72 4e
platform caam_sm: [0048] b9 ce 56 59 3c 9e 86 7a
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] d4 b9 5c f1 58 ab 1b 12
platform caam_sm: [0008] 7b 18 b4 09 7e 7c 4d a9
platform caam_sm: [0016] 0c 7f a3 6e f4 63 39 5b
platform caam_sm: [0024] a9 c4 e1 12 6f 03 23 ca
platform caam_sm: [0032] d6 16 2f df b3 b9 67 5d
platform caam_sm: [0040] 4d d4 1c f5 dc ae f5 80
platform caam_sm: [0048] 44 2d 42 d9 99 7c 16 fd
platform caam_sm: [0056] c6 e8 9e e5 2d db 54 27
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 25 7d 70 0f 3d 38 f8 b7
platform caam_sm: [0008] 6a 9c f3 40 f5 17 b5 ac
platform caam_sm: [0016] d9 f8 45 03 77 75 c5 22
platform caam_sm: [0024] 0b 7d d8 12 f5 24 66 20
platform caam_sm: [0032] 28 33 f1 e9 0e 84 b3 7b
platform caam_sm: [0040] 09 fb dc ea db c4 3e 38
platform caam_sm: [0048] e9 c0 a9 2c 2e 5a e9 e7
platform caam_sm: [0056] a2 77 ef de ea 29 75 da
platform caam_sm: [0064] 51 c7 dd 5a 51 d5 6f 0b
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] b8 c4 aa c3 76 5e 8a 87
platform caam_sm: [0008] 75 5c bb 18 b9 0f e9 d5
platform caam_sm: [0016] b5 49 14 fa 34 6d 1a c1
platform caam_sm: [0024] 30 af 9a 0d bc ef 70 79
platform caam_sm: [0032] 6f 5c 12 61 f4 6b b1 ef
platform caam_sm: [0040] 25 2c 73 c8 22 83 05 50
platform caam_sm: [0048] 31 dd a7 18 82 4d 47 69
platform caam_sm: [0056] 2f 56 61 e0 21 2d 8d 74
platform caam_sm: [0064] e5 ca 72 bc 27 49 33 78
platform caam_sm: [0072] 5a 07 f7 a9 8a b2 11 33
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] ca 69 a8 b6 a4 a5 71 f3
platform caam_sm: [0008] 9f d4 4f ff 78 67 46 63
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] a3 b0 d4 cd 25 7c 93 85
platform caam_sm: [0008] 11 e3 6d 53 b3 61 d8 fd
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] d0 95 82 89 34 00 89 d2
platform caam_sm: [0008] 45 f9 f6 13 80 46 30 e8
platform caam_sm: [0016] be 9d d4 5c 90 a9 90 2b
platform caam_sm: [0024] 41 5d 24 1e 62 da 9e 70
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 64 10 86 14 9a ac c4 99
platform caam_sm: [0008] 0d 9e c1 1d eb dd d1 5f
platform caam_sm: [0016] 33 0f f0 e2 93 2a aa 13
platform caam_sm: [0024] d8 21 94 51 90 49 3f 76
caam-snvs 20cc000.caam-snvs: can't get snvs clock
caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
usbcore: registered new interface driver snd-usb-audio
wm8962 0-001a: Failed to read ID register
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
fsl-hdmi-dai soc:hdmi_audio@00120000: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of soc:hdmi_audio@00120000 failed with error -12
imx-wm8962 sound: failed to find codec platform device
imx-wm8962: probe of sound failed with error -22
imx-audio-hdmi sound-hdmi: initialize HDMI-audio failed. load HDMI-video first!
NET: Registered protocol family 26
u32 classifier
    Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
IPv4 over IPsec tunneling driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
Segment Routing with IPv6
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
registered taskstats version 1
input: gpio-keys as /devices/soc0/gpio-keys/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:42:49 UTC (2569)
usb_otg_vbus: disabling
wm8962-supply: disabling
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 1024K
init: init first stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
init: [libfs_mgr]fs_mgr_read_fstab_default(): failed to find device default fstab
init: [libfs_mgr]Returning avb_handle with status: 0
init: [libfs_mgr]Loading verity table: '1 /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/system /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/system 4096 4096 451493 451493 sha1 8e6e0aacd5eaf2a09b9e9a82a9c66db008ef076b 44d3861d950db941fa585a5d90f0c5e6fc9ad8e2 10 use_fec_from_device /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/system fec_roots 2 fec_blocks 455050 fec_start 455050 restart_on_corruption ignore_zero_blocks'
EXT4-fs (dm-0): mounted filesystem without journal. Opts: barrier=1,inode_readahead_blks=8
init: [libfs_mgr]__mount(source=/dev/block/dm-0,target=/system,type=ext4)=0: Success
init: [libfs_mgr]Loading verity table: '1 /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/vendor /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/vendor 4096 4096 28199 28199 sha1 bd23f6c3a10e40531d7acd17619291ac95a8c56f 9bc512123f59449d5ec303b6594dd9ff6bf7a466 10 use_fec_from_device /dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/vendor fec_roots 2 fec_blocks 28423 fec_start 28423 restart_on_corruption ignore_zero_blocks'
EXT4-fs (dm-1): mounted filesystem without journal. Opts: barrier=1,inode_readahead_blks=8
init: [libfs_mgr]__mount(source=/dev/block/dm-1,target=/vendor,type=ext4)=0: Success
init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
init: Loading SELinux policy
SELinux:  Class process2 not defined in policy.
SELinux:  Class infiniband_pkey not defined in policy.
SELinux:  Class infiniband_endport not defined in policy.
SELinux: the above unknown classes and permissions will be denied
SELinux:  policy capability network_peer_controls=1
SELinux:  policy capability open_perms=1
SELinux:  policy capability extended_socket_class=1
SELinux:  policy capability always_check_network=0
SELinux:  policy capability cgroup_seclabel=0
SELinux:  policy capability nnp_nosuid_transition=0
audit: type=1403 audit(2570.230:2): policy loaded auid=4294967295 ses=4294967295
audit: type=1404 audit(2570.240:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
init: 2 output lines suppressed due to ratelimiting
init: init second stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
selinux: SELinux: Loaded file_contexts
init: Running restorecon...
init: waitid failed: No child processes
init: Couldn't load property file '/odm/default.prop': open() failed: No such file or directory: No such file or directory
init: Created socket '/dev/socket/property_service', mode 666, user 0, group 0
init: Forked subcontext for 'u:r:vendor_init:s0' with pid 213
init: Forked subcontext for 'u:r:vendor_init:s0' with pid 214
init: Mike: parseConfig /init.rc start: Success
audit: type=1400 audit(2570.600:4): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
ueventd: ueventd started!
audit: type=1400 audit(2570.600:5): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
selinux: SELinux: Loaded file_contexts
audit: type=1400 audit(2570.600:6): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
ueventd: Parsing file /ueventd.rc...
audit: type=1400 audit(2570.600:7): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
ueventd: Mike: path: /ueventd.rc, config_contents = subsystem adf
ueventd:     devname uevent_devname
ueventd:
ueventd: subsystem graphics
ueventd:     devname uevent_devpath
ueventd:     dirname /dev/graphics
ueventd:
audit: type=1400 audit(2570.700:8): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2570.700:9): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2570.700:10): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
imx-sdma 20ec000.sdma: loaded firmware 3.4
kauditd_printk_skb: 1 callbacks suppressed
audit: type=1400 audit(2571.050:12): avc:  denied  { write } for  pid=1 comm="init" name="alignment" dev="proc" ino=4026531987 scontext=u:r:init:s0 tcontext=u:object_r:proc:s0 tclass=file permissive=0
audit: type=1400 audit(2571.070:13): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
watchdogd: watchdogd started (interval 10, margin 20)!
audit: type=1400 audit(2571.070:14): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2571.070:15): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2571.070:16): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
Console: switching to colour dummy device 80x30
brcmfmac: Unknown symbol cfg80211_sched_scan_results (err 0)
brcmfmac: Unknown symbol cfg80211_scan_done (err 0)
brcmfmac: Unknown symbol cfg80211_sched_scan_stopped (err 0)
brcmfmac: Unknown symbol cfg80211_remain_on_channel_expired (err 0)
brcmfmac: Unknown symbol cfg80211_new_sta (err 0)
brcmfmac: Unknown symbol cfg80211_disconnected (err 0)
brcmfmac: Unknown symbol wiphy_new_nm (err 0)
brcmfmac: Unknown symbol cfg80211_ready_on_channel (err 0)
brcmfmac: Unknown symbol cfg80211_classify8021d (err 0)
brcmfmac: Unknown symbol cfg80211_crit_proto_stopped (err 0)
brcmfmac: Unknown symbol wiphy_register (err 0)
brcmfmac: Unknown symbol __cfg80211_alloc_reply_skb (err 0)
brcmfmac: Unknown symbol cfg80211_put_bss (err 0)
brcmfmac: Unknown symbol cfg80211_roamed (err 0)
brcmfmac: Unknown symbol cfg80211_check_combinations (err 0)
brcmfmac: Unknown symbol cfg80211_ibss_joined (err 0)
brcmfmac: Unknown symbol cfg80211_michael_mic_failure (err 0)
brcmfmac: Unknown symbol wiphy_apply_custom_regulatory (err 0)
brcmfmac: Unknown symbol ieee80211_get_channel (err 0)
brcmfmac: Unknown symbol cfg80211_del_sta_sinfo (err 0)
brcmfmac: Unknown symbol wiphy_unregister (err 0)
brcmfmac: Unknown symbol wiphy_read_of_freq_limits (err 0)
brcmfmac: Unknown symbol cfg80211_vendor_cmd_reply (err 0)
brcmfmac: Unknown symbol cfg80211_mgmt_tx_status (err 0)
brcmfmac: Unknown symbol cfg80211_unregister_wdev (err 0)
brcmfmac: Unknown symbol ieee80211_channel_to_frequency (err 0)
brcmfmac: Unknown symbol cfg80211_rx_mgmt (err 0)
brcmfmac: Unknown symbol cfg80211_report_wowlan_wakeup (err 0)
brcmfmac: Unknown symbol cfg80211_get_p2p_attr (err 0)
brcmfmac: Unknown symbol cfg80211_inform_bss_data (err 0)
brcmfmac: Unknown symbol ieee80211_frequency_to_channel (err 0)
brcmfmac: Unknown symbol cfg80211_connect_done (err 0)
brcmfmac: Unknown symbol wiphy_free (err 0)
random: crng init done
mke2fs: mke2fs 1.43.3 (04-Sep-2016)
mke2fs: Discarding device blocks:    4096/1184768 1052672/1184768                done                           
mke2fs: Creating filesystem with 1184768 4k blocks and 296592 inodes
mke2fs: Filesystem UUID: e4de33e7-fae0-443c-a427-7038e522b45b
mke2fs: Superblock backups stored on blocks:
mke2fs:  32768, 98304, 163840, 229376, 294912, 819200, 884736
mke2fs:
mke2fs: Allocating group tables:  0/37      done                           
mke2fs: Writing inode tables:  0/37      done                           
mke2fs: Creating journal (16384 blocks): done
init: [libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/userdata
init: [libfs_mgr]Enabling quotas on /dev/block/by-name/userdata
EXT4-fs (mmcblk0p11): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk0p11): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
init: [libfs_mgr]check_fs(): mount(/dev/block/by-name/userdata,/data,ext4)=0: Success
init: [libfs_mgr]check_fs(): unmount(/data) succeeded
init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/by-name/userdata
init: [libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/userdata
init: [libfs_mgr]Reserved blocks 32768 is too large; capping to 23695
init: [libfs_mgr]Setting reserved block count on /dev/block/by-name/userdata to 23695
init: [libfs_mgr]Enabling ext4 encryption on /dev/block/by-name/userdata
EXT4-fs (mmcblk0p11): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk0p11): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
init: [libfs_mgr]__mount(source=/dev/block/by-name/userdata,target=/data,type=ext4)=0: Success
mke2fs: mke2fs 1.43.3 (04-Sep-2016)
mke2fs: Discarding device blocks:   4096/131072              done                           
mke2fs: Creating filesystem with 131072 4k blocks and 32768 inodes
mke2fs: Filesystem UUID: d30abcd1-af53-4bbe-8f02-19baa606cd1d
mke2fs: Superblock backups stored on blocks:
mke2fs:  32768, 98304
mke2fs:
mke2fs: Allocating group tables: 0/4    done                           
mke2fs: Writing inode tables: 0/4    done                           
mke2fs: Creating journal (4096 blocks): done
init: [libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/cache
EXT4-fs (mmcblk0p5): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
init: [libfs_mgr]__mount(source=/dev/block/by-name/cache,target=/cache,type=ext4)=0: Success
init: 18 output lines suppressed due to ratelimiting
init: Parsing file /product/etc/init...
init: Unable to read config file '/product/etc/init': open() failed: No such file or directory
init: Parsing file /odm/etc/init...
init: Unable to read config file '/odm/etc/init': open() failed: No such file or directory
init: Keyring created with id 13666740 in process 1
init: Command 'mount_all /vendor/etc/fstab.freescale' action=fs (/vendor/etc/init/hw/init.freescale.rc:227) took 23088ms and succeeded
init: Service 'early_init_sh' (pid 216) exited with status 0
init: processing action (fs) from (/system/etc/init/logd.rc:18)
audit: type=1400 audit(2594.320:17): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:18): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:19): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:20): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:21): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:22): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:23): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:24): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:25): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
audit: type=1400 audit(2594.320:26): avc:  denied  { dac_read_search } for  pid=1 comm="init" capability=2  scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
zram0: detected capacity change from 0 to 536870912
logd.auditd: start
mkswap: Swapspace size: 524284k, UUID=ce842e72-bb06-4ef9-8070-bad3911861b1
Adding 524284k swap on /dev/block/zram0.  Priority:-2 extents:1 across:524284k SS
type=1400 audit(2594.600:47): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
fscrypt: Adiantum using implementation "adiantum(xchacha12-neon,aes-arm,nhpoly1305-neon)"
type=1400 audit(2594.620:55): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0 duplicate messages suppressed
type=1400 audit(2595.660:134): avc: denied { dac_read_search } for pid=256 comm="Binder:256_3" capability=2 scontext=u:r:vold:s0 tcontext=u:r:vold:s0 tclass=capability permissive=0
rfkill: BT RF going to : off
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
logd.daemon: reinit
using random self ethernet address
using random host ethernet address
file system registered
healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
type=1400 audit(2595.660:138): avc: denied { dac_read_search } for pid=256 comm="Binder:256_3" capability=2 scontext=u:r:vold:s0 tcontext=u:r:vold:s0 tclass=capability permissive=0 duplicate messages suppressed
type=1400 audit(2596.710:502): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0
sabresd_6dq:/ $ type=1400 audit(2596.710:506): avc: denied { dac_read_search } for pid=1 comm="init" capability=2 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=0 duplicate messages suppressed
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
read descriptors
read strings
type=1400 audit(2597.770:581): avc: denied { dac_read_search } for pid=316 comm="installd" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
type=1400 audit(2597.770:581): avc: denied { dac_read_search } for pid=316 comm="installd" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
android_work: sent uevent USB_STATE=CONNECTED
android_work: sent uevent USB_STATE=DISCONNECTED
android_work: sent uevent USB_STATE=CONNECTED
configfs-gadget gadget: high-speed config #1: b
android_work: sent uevent USB_STATE=CONFIGURED
Labels (1)
0 Kudos
Reply
2 Replies

930 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

one can try with Demo Image

Demo Images –i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI Boards and Platforms

use Android P9.0.0_2.2.0 Documentation for writing images.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

930 Views
zhangmike
Contributor II

Hi Igorpadykov:

    When I use uuu_imx_android_flash.sh script to flash the demo Images, it' failed.

untitled.png

0 Kudos
Reply