I have added two design-kits downloaded from the official website to ADS, but ADS still shows errors
解決済! 解決策の投稿を見る。
Thank you
This appears to be customer not installing RF High power Model Kit before using single product model.
Our models are two part :
RF High power Model Kit
Product Model Design Kit
Both parts are required to simulate device
Please, refer to:
https://www.nxp.com/docs/en/company-information/OVERVIEW_MDL_ADS_DESIGN_KIT.pdf
If this is not the case, please try with an earlier version of ADS 2019 or 2020.
Thank you
This appears to be customer not installing RF High power Model Kit before using single product model.
Our models are two part :
RF High power Model Kit
Product Model Design Kit
Both parts are required to simulate device
Please, refer to:
https://www.nxp.com/docs/en/company-information/OVERVIEW_MDL_ADS_DESIGN_KIT.pdf
If this is not the case, please try with an earlier version of ADS 2019 or 2020.
Do we have
I try two different design-kits AFT27S010N AFT09MS031N.
It shows same Error.
Warning detected by hpeesofsim during netlist parsing.
Model `FSL_AFT27S010N_FET2.FET2M1' (defined in file 'D:/ADS/helmholtz_wrk/AFT27S010N_Level2_Rev0_DK//circuit/models/fsl_AFT27S010N_pkg_netlists.net' around line 27): `FSLRFPK_FET2' is an undefined primitive device.
Warning detected by hpeesofsim during netlist flattening.
Resistor `FET2FSL1.R1' is shorted.
Error detected by hpeesofsim during netlist flattening.
`FSL_AFT27S010N_FET2.FSL1' is an instance of an undefined model `FET2M1'.
Hello,
I can not see the image, can you paste the image in your post or copy and paste the error, please?
Regards.