communications converter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

communications converter

594件の閲覧回数
CAM1956
Contributor I
Christine good morning, many thanks for your response. I believe I owe you a better expanation of what I am looking for:
 
I have a set of instruments wich communicate with my datalogger/gateway by means of IEEE 802.15.4, the data lgger then send the signal to a Modem and it goes into ur server.
 
A client wants me to have all data transmitted by cable, therefore I am looking for a device that can capture the radio signal (802.15.4) and convertes into something I can deliver through Fiber optics to my local server on site.
 
We also have several instruments that deliver the data via WiFi, I am also looking for anything that can be placed next to the instrument (in the same cabinet) that captures the wifi transmision and converts into data to be trabnsmitted over Fiber.
 
The whatever devise you may find as an option will be 9in a cabinet IP67 out in the field with temp -15°C to +45°C. aneregy supply to be 12/24VDC or 220VAC.
 
regards and again many thanks
 
Carlos
 
NC
 
0 件の賞賛
返信
0 返答(返信)