clrc663Plus Change a RxThreshold ISO/IEC14443-A 106

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

clrc663Plus Change a RxThreshold ISO/IEC14443-A 106

1,389件の閲覧回数
vincentthivent
Contributor III
Hi guys,

I want to optimize my nfc reader, how to change a default value into register RxThreshold with a NXP NFC Reader Library?

Thanks,
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to  9.12.4 RxThreshold of the datasheet as the link.

URL:https://www.nxp.com/docs/en/data-sheet/CLRC663.pdf.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信