boot issue with LS1028ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot issue with LS1028ARDB

2,597 Views
cm1
Contributor I

Hi everyone,

I used nxp_LS1028ardb. And I did SDcardboot up with ubuntu 20.04 while following Open Industrial User Guide rev1.10(12/2020).

When I start the board, some "failed" commands come up.(the log is attached)

Should I need to install anything additionally after SDcardboot? what I have to do to resolve the errors?

Thanks for your help.

cm1_5-1632832644795.pngcm1_5-1632832644795.png

cm1_1-1632832504881.pngcm1_1-1632832504881.pngcm1_2-1632832528051.pngcm1_2-1632832528051.png

cm1_3-1632832587816.pngcm1_3-1632832587816.pngcm1_4-1632832615408.pngcm1_4-1632832615408.png

 

0 Kudos
Reply
1 Reply

2,571 Views
ufedor
NXP Employee
NXP Employee
0 Kudos
Reply