bdi3000 configuration for MPC8313E-RDB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bdi3000 configuration for MPC8313E-RDB?

Jump to solution
4,316 Views
MartinL
Contributor I

Hi,

 

Does anyone have a working bdi2000/3000 configuration for the MPC8313E-RDB (rev c) dev. board?

 

I need it to have DDR and NOR flash support so that I can flash a new bootloader into NOR.

 

Thanks.

 

Br, Martin 

0 Kudos
Reply
1 Solution
3,231 Views
TedMarshall
Contributor II

I believe the attached should work.  I was working with a borrowed BDI2000 (which I no longer have) and later with it on a custom board bit I believe this will work with the RDB.

 

BTW, you don't need SDRAM to program the flash.  Using the workspace should speed it up but I was never able to get programming to work with the workspace, even with SDRAM properly configured.

 

Good luck.

 

bdi-mpc8313erdb.zip

Message Edited by t.dowe on 2009-11-08 10:29 PM

View solution in original post

0 Kudos
Reply
4 Replies
3,232 Views
TedMarshall
Contributor II

I believe the attached should work.  I was working with a borrowed BDI2000 (which I no longer have) and later with it on a custom board bit I believe this will work with the RDB.

 

BTW, you don't need SDRAM to program the flash.  Using the workspace should speed it up but I was never able to get programming to work with the workspace, even with SDRAM properly configured.

 

Good luck.

 

bdi-mpc8313erdb.zip

Message Edited by t.dowe on 2009-11-08 10:29 PM
0 Kudos
Reply
2,989 Views
precisionman
Contributor I

hi,

i'm looking for the configure file for mpc8313e

bdi-mpc8313erdb.zip

do you still have it? 

thanks a million.

tim

 

0 Kudos
Reply
3,231 Views
MartinL
Contributor I

Thanks for the configuration!

 

Flash programming worked like a charm - even without SDRAM configured. Apparently the default workspace is ok with the bdi3000.

0 Kudos
Reply
2,990 Views
precisionman
Contributor I

hi,

i'm looking for configure file for mpc8313e : bdi-mpc8313erdb.zip 

do you still have this file?

greatly appreciated.

thx, Tim

0 Kudos
Reply