Which board has....:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which board has....:

4,379件の閲覧回数
joe_K
Contributor I
Hey guys,
I'm looking for an ARM9 based development board, which must have:
32bit ARM9 MPU
Ethernet (10M as minimum),
USB (Host and device)
2 or 3 serial ports
LEDs and buttons
Linux support
better would it be if it has been assembled with a TFT LCD (3.5" or bigger") and come with pre-configured tool chain, binaries and source code.

Someone who has experience with such a thing please give me some recommendation, Thanks in advance
0 件の賞賛
返信
4 返答(返信)

3,312件の閲覧回数
joe_K
Contributor I
Thanks, but....
$2999.00 ??
GOD, I don't think I can afford that.
Any other ?
0 件の賞賛
返信

3,312件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
0 件の賞賛
返信

3,312件の閲覧回数
leon2008
Contributor I
The taskit Panel-Card seems good.
And beside this, the MINI2440 + LCD from http://www.developmentboard.net fits your requirements too,

Samsung S3C2440 (ARM920T) MPU
64M SDRAM, 64MB NAND flash, 2M Nor Flash
32bit data bus
ethernet, 2 x USB, 3 x serial port
3.5" LCD....

Euro200 only

check them out, might be interesting
0 件の賞賛
返信

3,312件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
 
Regards,
 
Fabio Estevam
0 件の賞賛
返信