What's this command mean?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's this command mean?

3,252件の閲覧回数
CaoJason
Contributor I
Hello:
       Who can give me the detail explain about" FORCEACTIVE { gInterruptVectorTable, __reset, __ext_int, __decr, __machine_check }"
      This command is in the link file MPC564EVB_ROM.lcf.
thanks!
0 件の賞賛
返信
4 返答(返信)

2,237件の閲覧回数
CrasyCat
Specialist III
Hello
 
This commands disable dead stripping for the symbols gInterruptVectorTable, __reset, __ext_int, __decr, __machine_check.
That means that the symbols enumerated above will be linked to the application even though they are not referenced in there.
 
CrasyCat
0 件の賞賛
返信

2,237件の閲覧回数
CaoJason
Contributor I
Hi Cat:
     In the file,the __reset, __ext_int, __decr, __machine_check are the function dealing exception,That means function cann't be used to deal some application if it is  not listed in FORCEACTIVE{} 
    Another question: .equ vec_base 0x3FE000,what does this sentence mean?
0 件の賞賛
返信

2,237件の閲覧回数
CrasyCat
Specialist III
Hello
 
The problem with interrupt function is that they are not explicitly called in the application. So if you do not specify them in a FORCEACTIVE command they may not be linked with the application.
 
Usually one would create a constant table of function pointer for the interrupt table and then specify the table in the FORCEACTIVE command. This would make sure that all interrupt functions, which address is specified in the table gets linked to the application.
 
The statement .equ vec_base 0x3FE000 is probably stored somewhere in an assembly source file.
It associates the value 0x3FE000.to symbol vec_base.
 
So each time you will use vec_base  in your assembly source file, assembler will replace that with 0x3FE000.
 
CrasyCat
0 件の賞賛
返信

2,237件の閲覧回数
CaoJason
Contributor I
Thanks Cat,I get it.
0 件の賞賛
返信