What is a Hawk?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is a Hawk?

Jump to solution
2,663 Views
GaryOlmstead
Senior Contributor I

Hi --

 

One of your USB TAP debuggers is specified as being for the Hawk.  So, which processors are those?

0 Kudos
Reply
1 Solution
1,884 Views
GaryOlmstead
Senior Contributor I

Christian --

 

Your first link is broken, but it doesn't matter. 

 

I decided to risk the $99, and ordered it.  It works OK.

 

For anybody contemplating a USB TAP debugger, you set it up by selecting Edit (target) Settings Remote Debugging Connection, where  (target) is the name of your project, as selected in Project Set Default Target. 

 

DO NOT use Edit Preferences Remote Connections They offer the same choices, but only the first one actually does anything useful.

View solution in original post

0 Kudos
Reply
2 Replies
1,884 Views
clangen
Contributor I

'Hawk'  is the alias name for the DSP56(F)8xx hybrid (DSP+MCU) series, see:

 

http://www.freescale.com/webapp/sps/site/overview.jsp?code=DSC_HOME.

 

They use the OnCE (On Chip Emulator) debug interface like the DSP563xx (Onyx) and DSP5672x series. I guess you got the 'Hawk' alias name from here:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=USBTAP&tab=Buy_Parametric_Tab&fromSea...

 

Anyway the Code Warrior USB Tap is only usable for the speciefied MCU and the according Code Warrior tool.

 

Best regards

 

Christian

 

0 Kudos
Reply
1,885 Views
GaryOlmstead
Senior Contributor I

Christian --

 

Your first link is broken, but it doesn't matter. 

 

I decided to risk the $99, and ordered it.  It works OK.

 

For anybody contemplating a USB TAP debugger, you set it up by selecting Edit (target) Settings Remote Debugging Connection, where  (target) is the name of your project, as selected in Project Set Default Target. 

 

DO NOT use Edit Preferences Remote Connections They offer the same choices, but only the first one actually does anything useful.

0 Kudos
Reply