WCT1013A-15W bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WCT1013A-15W bootloader

2,154 Views
2194133213
Contributor I

Hi
   NXP official website WCT1013a BootLoader routine is through the serial port.Now I want to change the serial port mode to CAN communication mode based on the routine bootloader.Now I port the can.c file and can.h of WCT1013a(demo) application into the BootLoader.But CAN communication is always unsuccessful. What should I do?
   Who can help me, thank you very much.

Labels (3)
0 Kudos
Reply
1 Reply

1,838 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you refer to the CAN example

C:\CW MCU v11.0\MCU\CodeWarrior_Examples\Processor_Expert\DSC\TWR-56F8400\CAN

After you can read the CAN frame, then develop the bootloader code.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply