Using PCA9548A with upstream slave (after configuration)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using PCA9548A with upstream slave (after configuration)

1,375件の閲覧回数
twolfe
Contributor I

We are trying to use the PCA9548A with a downstream master device.  Is it possible to use the upstream master to configure the Control Block to connect to the downstream master, then after this configuration, reconfigure the upstream device to be a slave such that the downstream master can write data to the upstream slave?  Based on the PCA9548A block diagram and app note, the PCA9548A operates like a wire after configuration with clock/data able to go in either direction.  Do you see any issues with this plan? 

Thanks, Ted

タグ(1)
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Could you please give us your application simple diagram?

0 件の賞賛
返信