Using PCA9548A with upstream slave (after configuration)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using PCA9548A with upstream slave (after configuration)

1,378 次查看
twolfe
Contributor I

We are trying to use the PCA9548A with a downstream master device.  Is it possible to use the upstream master to configure the Control Block to connect to the downstream master, then after this configuration, reconfigure the upstream device to be a slave such that the downstream master can write data to the upstream slave?  Based on the PCA9548A block diagram and app note, the PCA9548A operates like a wire after configuration with clock/data able to go in either direction.  Do you see any issues with this plan? 

Thanks, Ted

标记 (1)
0 项奖励
回复
1 回复

1,367 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Could you please give us your application simple diagram?

0 项奖励
回复