Use of Ringo software in tea2017?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use of Ringo software in tea2017?

2,096 Views
Jayler
Contributor I

1. Can the new TEA2017 chip be used directly without software configuration?

2. There are two groups of signals from I2C, which are connected to the device and the development board. What is the difference between the two in software configuration?

3. Is there any other way to buy rdk01db1563 in China? The official website has been sold out.

0 Kudos
Reply
3 Replies

2,093 Views
guoweisun
NXP TechSupport
NXP TechSupport

1: Yes,you can!
2:which point do you mean? 

3:contact with your local NXP distributors:Distributor Network | NXP Semiconductors

0 Kudos
Reply

2,089 Views
Jayler
Contributor I

about 2:I can configure tea2017 with tea2017dk1002 or directly on the  power board. What is the difference between the two methods?

thank you!

0 Kudos
Reply

2,074 Views
guoweisun
NXP TechSupport
NXP TechSupport

Depend on your side,you also can directly program it in your power board.

0 Kudos
Reply